This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV07A: 3.3V to 5V Buffer finding

Part Number: SN74LV07A
Other Parts Discussed in Thread: SN74AHCT244

Hi TI EE

             Please help to suggest a Buffer.

             5V VCC,and have the function to change 3.3V Voltage level  to 5V Voltage level.Not Open Collector. And do not need pull up .5V output driver current at least 8mA .Thank You.

Regards

Cheney_Sun

  • Hello Cheney,
    I understand that you are looking for a buffer that will be supplied from 5V, but will be taking 3.3V inputs, and you do not want an open-collector (or open-drain) solution. The IOH needs to be at least 8mA @ 5V, 0.5V drop.

    I think the SN74AHCT244 will do what you want.