This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How do I terminate any unused channels of a logic device?

Guru 55530 points

Replies: 0

Views: 776

All CMOS inputs must be terminated at either Vcc or Ground.

The inputs of a CMOS device are high-impedance.  These terminations can be through a resistor (for example, a 10kohm pull-up resistor to Vcc or a 1kohm pull-down resistor to ground), or they can be directly connected. 

CMOS outputs are typically best left floating.  If this is not an option (for example, in transceivers where inputs and outputs share a pin), the output can be terminated to ground or Vcc through a resistor (10k, 100k, etc).


Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.