Hello to All,
Thank you for taking time to consider my problem. I have set the TXB0304 as a level translator between a Raspberry pi zero W and an ICM20948, inertial sensor by TDK, formerly Invensense. The TXB0304 circuit is very simple in that it only has two capacitors in the circuit for bypassing both the VCCA and the VCCB. The signal lines are translated from one voltage to other, while the I2C lines out of the master, Pi, are present at the B "inputs" they do not appear at the "output" of A. The signal at the B ports looks as expected with an oscilloscope, but the scoped ports of A are without any indication that port B is toggling. The OE signal of the TXB0304RUTR has either a pullup or pulldown and have used both with a 4k7 ohm resistor but neither creates an enabled translator?
Thank you!
Cy Drollinger