Other Parts Discussed in Thread: SN74LVC1G17, SN74LVC2G17
Dear Support,
I am trying figure out how many loads can the SN74AUP1G17DBVR drive. I am seeing weird behavior using other vendors.
Here is our circuit on U21 with NC7SP17P5X (2.6 mA at 3V) driving 3 loads.
Please see attachment.NC7SP17P5X_Load_Drive_Capbility.pdf
Questions?
- Why is the output (red trace) did not go directly to 3V but has a step to 1.2V then 2.2V? It sometimes hang at 1.2V and never drive up to to high 2.2V.
- Is this a load driving issue?
- Do you have a load calculation application notes on how to figure out if 2.6 mA or 4mA is sufficient to drive the 3 loads?
- Will replacing 4mA device SN74AUP1G17 resolve this issue?
Please advice.
Thank you.
Regards,
Randy