This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCT74: Switching characteristics vs. temperature

Part Number: SN74HCT74
Other Parts Discussed in Thread: SN54HCT74

In the datasheet for the SN74HCT74, page 4 shows a table for "over recommended operating free-air temperature range." There are three columns including "TA = 25°C", "SN54HCT74," and "SN74HCT74."

I understand that each of the "SNxxxxxxx" columns are showing the maximum switching times for the overall temperature ranges (-55 ~ 125°C and -40 ~ 85°C), and "TA" is giving typical and max for room temperature (25°C), but is there a plot to show how changes in temperature change the switching times? Or at least something basic like that switching time increases or decreases with heat?

Here's the datasheet I'm looking at: http://www.ti.com/lit/ds/symlink/sn74hct74.pdf

Thanks,

Mike