This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] This standard logic datasheet says "automotive qualified" but not AEC-Q100 qualified. What does it mean?

Guru 55210 points

Replies: 0

Views: 717

Some of our older datasheets still just say “qualified for automotive applications” – however all of our automotive parts are tested in accordance with AEC-Q100 requirements.

 

The Automotive Electronics Council (AEC) Component Technical Committee defines the standard (as of this writing, AEC-Q100, Rev H) that semiconductor devices must meet or exceed to be labelled as “AEC-Q100 qualified,” however they do not travel from company to company individually certifying every device that is in production.  They are just a standards organization, consisting of members from top automotive manufacturers and semiconductor companies worldwide (see this website for a current list of members: http://www.aecouncil.com/index.html ). It is up to the individual manufacturer to ensure that parts are tested correctly and that they meet the standards put forth by the AEC.

Texas Instruments is a member of the AEC, and thus every part that we label as “automotive qualified” is certified by a company that is on the council.


Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.