This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What should be done with unused I/O pins of the level translator devices?

Mastermind 49830 points

Replies: 0

Views: 658

For the TXB family, unused I/O ports are recommended to be tied to GND through a weak pulldown resistors (>=100kohm).

For TXS devices, the internal 10kohm pull-ups resistors will ensure that the I/O ports are never floating and hence can be left disconnected.

For LSF devices, the unused I/O ports can be left disconnected as they are passive switch type translators.

For AVC/LVC devices, the unused input and output ports are recommended to be tied to gnd.

For AXC devices, the unused input and output ports can be left unconnected as there are very weak pulldown resistors internally. This helps in avoiding unknown voltages at the pins thus reducing the power consumption due to floating voltage levels.

-Thanks,

Shreyas

Watch the Introduction to AXC Family

Read the app note on Glitch-free Power Sequencing for the AXC family

Evaluate the AXC8T245 EVM and watch the translation using the EVM