Other Parts Discussed in Thread: SN74AC244
Can I gang 4 of these together to increase current drive (trying to drive a 15meter cable), or do we get contention issue due to part-part input to output prop delay.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I gang 4 of these together to increase current drive (trying to drive a 15meter cable), or do we get contention issue due to part-part input to output prop delay.
It is possible to gang CMOS outputs together to get more drive strength, but you should do this only for outputs on the same device.
I am guessing that you have chosen the SN74LVC2G34 because you want symmetric drive strength and are running at 5 V. Under these assumptions, you can use buffers in the AC family.
With 15 m cables, consider using differential signals.
Hi Clemens,
Thank you for your reply. The other end of the cable is single ended buffer, and I don't have the leverage to chnage that design, therefore got to go with single ended driver.
2 gates are not sufficient, we need over 100 Ma to stay within the required rise and fall, please suggest a 4 gate part.
Why AC family, max sink and source is 24mA, isn't it? Please explain why AC family!?
Thanks,
Bahram
As I said, the AC family can run at 5 V and has symmetric drive strength.
Are you running at 5 V?
Hi Bahram,
The AC family is a suitable suggestion for this. Even though the outputs can be tied together for higher drive, it is important to still stay under the abs max current through the VCC and GND pins. This family has devices that have a higher current ratings than 100 mA to meet your needs.
Are you suggesting to use a SN74AC244 part? So ganging all inputs therefore outputs together should be fine and give enough current. I am placing a 39ohms series driving the cable, therefore max sink/source would be around 125mA. What is the gates output impedance for SN74AC244?
Thanks,
Bahram
Hi Bahram,
You can find out how to estimate the output impedance by referring to the FAQ below:
https://e2e.ti.com/support/logic/f/151/t/742466?tisearch=e2e-sitesearch&keymatch=faq%3Atrue