This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74HC595: fclock at Vcc=3.3V

Guru 16220 points

Replies: 2

Views: 122

Part Number: SN74HC595

Hi

There is timing requirement for clock frequency of SN74HC595 and SN54HC595 as follows.

My customer want to have maximum specification at Vcc=3.3V for both SN54HC595 and SN74HC595 devices.

Do you have information you can share to the customer?

BestRegards

  • Hello,

    It is fine to use linear interpolation on the given values in the datasheet to approximate your values for 3.3 V. 

    See this FAQ for more details on that. 

    regards,

    Gabriel

  • Guru 16220 points

    In reply to Gabriel Lake1:

    Hi Gabriel

    Thank you for your reply.

    According to formula provided in FAQ link, I got following estimation.

    54HC595 -> 10.96 MHz

    74HC595 -> 12.8 MHz

    BestRegards

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.