This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: there is no output on pins B if there are signals of input pins

Part Number: TXB0104

Hi,

I try to make TXB0104PW works with 3.3V SPI from STM32 and 1.8V IMU ICM-20948 but without success. I've re-soldered pins  B1 - B4, provided input signals for A1-A4  (doesn't matter high, low or 50% duty pulses). there are no signals on output pins. 1.8 and 3.3 voltages are connected correct. Please see attached schematic. 

Thanks,
Vasyl