This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TXS0104E: TXS0104E for I2C Level Translation and Pull Values

Prodigy 185 points

Replies: 9

Views: 216

Part Number: TXS0104E

Hi TI team,

We are using this part for I2C Level Translation.
Our Host Processor Works on 3.3V and Slave IC is on 1.8V.
That is why we used Level Translator in between.

This IC does have Internal 10K Pull up resistor but if my I2C Slave devices need the Lower Value of I2C Pull up, then shall I connect the Pull-up both the sides?

Regards
Saumil

  • It does not matter on which side you connect any additional pull-up resistors.

    But why do you need them? With the TXS's edge accelerators, it should never be necessary for speed reasons.

  • In reply to Clemens Ladisch:

    Hi Team,

    Let us say if my systems need only 2.2K Pull up value for the I2C and if I have used this level translators then how shall I use 2.2K as Pull up with this part?

    Regards

    Saumil

  • In reply to Saumil Shah60:

    The two internal 10 kΩ pull-up resistors are in parallel. To get the equivalent of 2.2 kΩ, add a 3.9 kΩ pull-up resistor.

    Again: what is the reason that your system needs 2.2 kΩ?

  • In reply to Clemens Ladisch:

    Hey Saumil,

    It isn't recommended to use additional pull-ups with this device. Could you explain why it needs to be a smaller pull-up?

    Check out our new AXC family of Voltage Translators! 

    Watch the Introduction to AXC Family to find out more about the family.

  • In reply to Dylan Hubbard:

    Hi,

    In this case,

    It is a Big Problem.

    I have connected total of 6 devices on the same I2C Lines.

    5 of them are working on the 3.3V and only one is working on 1.8V.

    Anyhow one side my I2C lines need the Pull up for the Other devices as well as we have calculated the Pull-up Values then it is Coming around 2.2K.

    It seems that in my case this Level translator is not usable.

    Regards

    Saumil

  • In reply to Saumil Shah60:

    Why do you think it is not usable? Does it not work when you are testing it?

    How did you calculate the 2.2 kΩ value? It is likely that the TXS's edge accelerators make your calculation invalid.

  • In reply to Clemens Ladisch:

    Hi Team,

    So Do you mean to say Shall we try without Pull-up with Level Translators?

    Regards

    Saumil

  • In reply to Saumil Shah60:

    Yes.

  • In reply to Clemens Ladisch:

    OK, We will try the same and get back.

    Regards

    Saumil

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.