This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 145
Part Number: LSF0204-Q1
Hi We faced an issue for UART_TX level translation that means the voltage level is kept on high always.(A/B side of level shift). It seems like the internal MOS doesn't work normally based on current setting. Current design is to place pull up 10K on B side of level shift only. In this case, we tried to change the pull up reisitance value up to 62Kohm to adjust a capable of driving current. The level shift can be workable but i'm afraid a such higher resistance value will increase the charge time.(Pull up lower than 51Kohm isn't workable) May I have your comments for this? Why the pull up 10Kohm can't turn on for level translation? Your feedback will be appreciated. Thanks. Please find the schematic&waveform for your reference.
The images did not attach; please try again.
What is the drive strengh of your other chip?
In reply to Clemens Ladisch:
Hi,
As Clemens mentioned, please provide the schematic. While we review it, I would recommend watching the following series on operating the LSF devices. You might find something to fix your issue.
https://training.ti.com/introduction-voltage-level-translation-lsf-family?cu=1134826
Thanks!
-Karan
In reply to Karan Kotadia:
Hi Karan,
The issue is solved. Thanks for your feedback.