Hi team,
SN74LS240NS shows hysteresis on the datasheet but it doesn't specify its threshold voltage.
Could you please provide each high→low and low→high threshold voltage?
Best regards,
Shota Mago
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
SN74LS240NS shows hysteresis on the datasheet but it doesn't specify its threshold voltage.
Could you please provide each high→low and low→high threshold voltage?
Best regards,
Shota Mago
Hi Karan-san
Thanks for your quick reply.
In accordance to datasheet, it shows that hysteresis voltage is 0.4V(typ).
So I think there is actual threshold voltage for each Low→High/High→Low which should be VT+ − VT-−=0.4V.
Is it possible to provide the actual threshold voltage if you have?
Best regards,
Shota Mago
The datasheet specifies the hysteresis, but not the absolute voltage of the thresholds. They can be anywhere between VIL and VIH.
Hi,
You should never be operating near the threshold voltages. The VIH and VIL specs I have given is what you should conform to when switching on the device. The hysteresis will help if the input signal has a slow rising or falling edge as the device will not falsely switch or oscillate at the output.
Thanks!
-Karan