Other Parts Discussed in Thread: TXS0102
Hello,
Regarding to VSIM* and SIM*I/O on TXS4558, my customer is asking some question.
(Question)
1)When EN*=H and Vcc=0, is VISM* off?
2) Do you have a data of VIL/VIH in SIM*I/O?
Regards,
Tao_2199
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tao,
Since the Logic circuitry is powered down, It shouldn't be able to start the activation sequence enabling the LDO output. Since this device uses similar level shifting architecture as the TXS0102, the customer can use the VIH/VIL values from that device using VSIMx as the supply.
Hi Tao,
This is correct. The Sim card will most likely drive the signal all the way to Vcc and ground so this shouldn't be an issue.