This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC1T45: Phase noise

Part Number: SN74AVC1T45
Other Parts Discussed in Thread: SN74AXC1T45

Hello Support team,

Are there specification or data of the phase noise of SN74AVC1T45?
Is it possible to achieve -135dBc/Hz@100kHz, -140dBc/Hz@1MHz with SN74AVC1T45?

Best Regards,
Hirokazu Takahashi

  • Hi Takahashi san,

    We do not specify any phase noise specs in the datasheet.

    However, We had measured RMS phase jitter on SN74AXC1T45 at 47.3ps at 25Mhz input source ( with RMS jitter 18.8ps).

    The additive RMS jitter of the SN74AXC1T45 is 28.5ps ( 47.3ps-18.8ps).

    Would this be sufficient for the application?

     

    -Thanks,

    Shreyas