Hi
Could you provide the data of pulse width variation over temperature ?
I found the application report SLVA720 which shows the variation between 10℃ - 85℃ but customer needs the data over temperature.
Thank you and best regards,
Michiaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you provide the data of pulse width variation over temperature ?
I found the application report SLVA720 which shows the variation between 10℃ - 85℃ but customer needs the data over temperature.
Thank you and best regards,
Michiaki
Hi Shreyas,
1. On the figure7 and figure8 in slva720.pdf.
Could you kindly advise the reason why the pulse duration is changed by temperature ?
In figure7, We see that the pulse duration is changed linearity at VCC=5.5V but it isn’t changed between 10℃ and 30℃ for the others.
Why is the above seen ?
2. Multiplier K
Is it correct that multiplier K is defined by capacitor size and supply voltage ?
Could you provide the multiplier K equation ?
Customer think that K and capacitor size would not be proportional.
3. Could you kindly advise the device that has smaller variation for Tw over temperature ?
4. I got the data customer measured.
Could you kindly review the data whether it is matched with the theory or not offline.
Thank you and best regards,
Michiaki
Hi Michiaki,
All the specs of the devices are affected by the process, temp and voltage and this is no different.
the graph shows that the temperature affect is very minimal and the pulse width duration is relatively stable with < 2% variation.
K can be found from the graph 5 and you are correct that the K varies depending on the cap values chosen.
I have requested this device expert to take a look and reply with additional information.
Hello Michiaki-san,
First, I would like to be clear that the SN74LVC1G123 is not a precision device. If extreme precision in timing is required, I would recommend against using it.
Michiaki Tanii said:1. On the figure7 and figure8 in slva720.pdf.
Could you kindly advise the reason why the pulse duration is changed by temperature ?
Pulse duration is dependent on many factors including, but not limited to: internal capacitance, comparator variation, reference variation, leakage current, internal delays. All of these have some dependence on temperature.
Michiaki Tanii said:In figure7, We see that the pulse duration is changed linearity at VCC=5.5V but it isn’t changed between 10℃ and 30℃ for the others.
Why is the above seen ?
Temperature change is part dependent - the device tested shows a relatively linear change across some temperatures, but this does not mean that all devices will have the exact same variation. The data is provided to show that there is minimal change over temperature, not to give a precise characterization for precision use.
Michiaki Tanii said:2. Multiplier K
Is it correct that multiplier K is defined by capacitor size and supply voltage ?
Yes, K is dependent on capacitor size and supply voltage, as well as temperature.
Michiaki Tanii said:Could you provide the multiplier K equation ?
Customer think that K and capacitor size would not be proportional.
K is determined experimentally - I do no have an equation to share for it.
K and timing capacitor size are not directly proportional, but they are related. For very large capacitance values, K becomes relatively constant. For small capacitance values, K changes significantly. This is related to the difference between the internal capacitance (which is non-linear) and the external capacitance.
Michiaki Tanii said:3. Could you kindly advise the device that has smaller variation for Tw over temperature ?
All monostable multivibrators have temperature dependence and are not designed for precision delays. I would recommend using a different method of timing for precision delays, such as a comparator + RC circuit, or a crystal + microcontroller.
Michiaki Tanii said:4. I got the data customer measured.
Could you kindly review the data whether it is matched with the theory or not offline.
I would be happy to review their data.
Hi Emrys,
Customer has the inquiries on the “4.1.1.1 Temperature Stability” in the application report slva720.pdf as below
Thank you and best regards,
Michiaki
Hi Michiaki-san,
Michiaki Tanii said:Customer has the inquiries on the “4.1.1.1 Temperature Stability” in the application report slva720.pdf as below
- Figure7 which conditions is Cext = 100pF shows the pulse width is around 57us at VCC=5.5V, 50℃ but pulse width is shorter at 14.5us in the Figure8 at same conditions with Figure7 even though the Cext is increased at 500pF.
Why is the pulse width longer ?
Looking at Figure9, pulse width is longer at 108us by increasing Cext compared with Figure7.- Compared between Figure9 and Figure7, pulse width is not 10 times even though Cext is 10 times.
Please advise the reason.
Thanks for bringing this to my attention. The images for Figure 7 and Figure 8 are reversed - this is an error in the application note that I will correct.
Hi Emrys,
Could you kindly the answer for the inquiry of 2. ?
Thank you and best regards,
Michiaki
Hi Michiaki-san,
I did answer this. Figure 7 and Figure 8 are switched. Compare Figure 9 with Figure 8 and you will see the expected ~10x difference.
1. If Figure 7 and Figure 8 are switched, we couldn’t see the 10x difference compared Figure 9 with Figure 8.
It is about 7.5x difference.
Could kindly advise why the change of Cext does not correspond with Tw ?
Tw = 14.4 us at Ta = 10℃, Cext = 100 pF and Tw = 107.5 us at Ta = 10℃, Cext = 1nF.
Cext is 10x difference but Tw is not 10x difference.
2. Could you share the Fig 7, 8, 9 at between -40℃ and 125℃ ?
3. In the case of fixed Rext = 100kohm, the rate of change for Tw is smaller if Cext is bigger.
Please advise the reason.
4. If Cext is fixied and Rext is larger, the rate of chage for Tw is smaller as well as the above case ?
5. Customer is considering to change Rext to 470kohm to get wide Tw by changing Cext.
if Rext * Cext is fixed, the change rate for Tw by temperature is same ?
For instance, in the case of the below conditions, the change rate of Tw by temperature is same ?
- Rext = 100kohm, Cext = 100pF
- Rext = 470kohm, Cext = 21.4pF
6. If supply voltage is 5V ± 2%, how variation for Tw is ?
if we could estimated variation, please let us know how to do.
Michiaki Tanii said:1. If Figure 7 and Figure 8 are switched, we couldn’t see the 10x difference compared Figure 9 with Figure 8.
It is about 7.5x difference.
Could kindly advise why the change of Cext does not correspond with Tw ?
Tw = 14.4 us at Ta = 10℃, Cext = 100 pF and Tw = 107.5 us at Ta = 10℃, Cext = 1nF.
Cext is 10x difference but Tw is not 10x difference.
There is also a K factor involved. The equation for pulse width is:
tw = K * R * C
For a 100pF capacitor, the K factor is significantly larger than it is for a 1000pF capacitor. In this case, K = 1.41 @ 5.5V for the 100pF capacitor, and K = 1.04 for the 1000pF capacitor.
Michiaki Tanii said:2. Could you share the Fig 7, 8, 9 at between -40℃ and 125℃ ?
No. All data that was taken is provided in the application report.
Michiaki Tanii said:3. In the case of fixed Rext = 100kohm, the rate of change for Tw is smaller if Cext is bigger.
Please advise the reason.
The K factor is primarily dependent on the internal capacitance of the device. With lower capacitor values, the internal capacitance has a larger effect on the external capacitor charge rate. With large devices, the effect is minimal and the K factor flattens out. As you can see in the datasheet, figure 6, the difference in K factor between a 0.1uF capacitor and a 0.01uF capacitor is very small, but when dropping to a 1000pF (0.001uF) capacitor, the change is more drastic.
Michiaki Tanii said:4. If Cext is fixied and Rext is larger, the rate of chage for Tw is smaller as well as the above case ?
If Cext is fixed and Rext is increased, the K factor will remain relatively constant. I say 'relatively' because there are still factors such as leakage that can affect operation of the device. I would recommend keeping timing resistors less than 1 Mohm to prevent a significant change in operation from leakage current (up to 0.25uA at the Rext/Cext pin).
Michiaki Tanii said:5. Customer is considering to change Rext to 470kohm to get wide Tw by changing Cext.
if Rext * Cext is fixed, the change rate for Tw by temperature is same ?
For instance, in the case of the below conditions, the change rate of Tw by temperature is same ?
- Rext = 100kohm, Cext = 100pF
- Rext = 470kohm, Cext = 21.4pF
I would expect to see similar performance across temperature to that shown in the application report. For a safety margin, I would recommend designing with +/- 5% tolerance.
I must repeat my previous recommendation - this is _not_ a precision device, and we cannot guarantee exact operation from one batch to another. Even if your customer extensively tests this device and proves that it works perfectly in their application, it is possible that next year a minor shift in process will result in different performance. We can only guarantee what is in the datasheet.
Michiaki Tanii said:6. If supply voltage is 5V ± 2%, how variation for Tw is ?
if we could estimated variation, please let us know how to do.
Hi Emrys,
Could you kindly share the variation, characteristic of temperature for internal capacitance value ?
The reason of inquiry is you mentioned that K factor is dependent on the internal capacitance value.
Thank you and best regards,
Michiaki