Hello,
I'm using this level-shifter so that my PIC18F4520 (5V - master - microcontroller ) can communicate with an LSMDS3H (3.3V - slave - inertial module) using SPI. Also, I have other slaves in my system which are not using any level shifting.
1) The inertial module has it's own chip select line, do I need to run that through the shifter?
2) My main question is regarding the OE pin; what size resistor do I need to use as a pulldown to ground? I'm having difficulties finding an answer in the datasheet.
- Maximum current sunk/sourced by any I/O pin on my microcontroller = 25mA
- Input leakage current for any I/O pin on my microcontroller = 200nA