Hi Team,
My customer is using TXB0104 now. And when port B get 3.3V signal, we would like to see 1.8V in port A. But we see 2V on the port and we also check the VCCA is 1.8V. I checked the datasheet and it showed that maximum of "Voltage applied to any output in the high or low state" is VCCA+0.5V. So I think 2V is normal. However customer could like to see the Port A is up to 2V. Do we have any suggest to make portA maintain in 1.8V or any solution could meet customer spec?
Roy