This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0206-29: Help to check TXS0206-29 package dimension details

Part Number: TXS0206-29

Hi Team,

Help to check the dimension size in data sheet P.24. Will it be ok if customer use 1.558 mm for E? =(1.588+1.528)/2.

Per customer feedback, the CAD limitation would be down to 3rd digits after decimal. it would be an issue using 1.5575 (1.588+1.527)/2. Thanks 

https://www.ti.com/lit/ds/symlink/txs0206-29.pdf

D: Max = 1.988 mm, Min = 1.928 mm

E: Max = 1.588 mm, Min = 1.527 mm