• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Logic » Logic Forum » All Tags » buffer
Share
Logic
  • Forums

Browse by Tags

Logic

Welcome to the Logic Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
buffer
  • 16374
  • 3.3V
  • 3.3V Output
  • 3-State
  • 5V
  • 5V tolerant
  • AVC
  • data sheet
  • datasheets
  • I2C
  • input transition rate
  • Interface
  • inverter
  • level conversion
  • Level Shifter
  • Level Translator
  • levels
  • Logic
  • Logic Level
  • logic level shifter
  • Mil
  • SN74LVC
  • spec
  • transition rate
  • voltage translator
Related Posts
  • Forum Post: SN74ALVC244 drive capacitance

    Paul Peterson52746 Paul Peterson52746
    I am looking at obtaining this part http://focus.ti.com/docs/prod/folders/print/sn74alvc244.html . However I can not find on the datasheet or on the web how much capacitance the buffer can drive. The current setup can drive approx 70 pF but when you add up the capacitance of the card and the coax we...
    on Jul 1, 2010
  • Forum Post: input transition rate SN74AUP3G17 vs. SN74AUP1G17

    Matthias Geipel Matthias Geipel
    Hello, according to the datasheets of the SN74AUP3G17 (triple buffer) and SN74AUP3G14 (triple inverter) a max. input transition rise/fall rate of 200ns/V is recommended, although these devices feature Schmitt trigger inputs . For the single gate (SN74AUP1G17 / SN74AUP1G14) and dual gate versions ...
    on Sep 15, 2010
  • Forum Post: ADC Data buffer needed for customer

    Sarah Pardee Sarah Pardee
    Here’s list of requirements for an ADC data buffer that my customer needs: 1.) Can either be one 32bit buffer IC, or two 16bit buffer IC’s (Note: Two 16bit buffers are somewhat preferred). 2.) In/Out frequency is 96MHz. 3.) In/Out Signal Type is CMOS @ 1.8V, and is unidirectional...
    on Nov 5, 2010
  • Forum Post: SN74LV8151 Input Voltage Tolerance

    Robert DeMott Robert DeMott
    Could someone confirm whether the SN74LV8151 inputs are 5V tolerant when operating from a 3.3V supply? The recommended operating conditions section of the datasheet seems to imply that they are (max input voltage of 5.5V), but this isn't explicitly stated in the part description. Thanks.
    on May 11, 2011
  • Forum Post: partial power down Ioff

    Dan-o Dan-o
    I am a little confused on partial power down Ioff. Is that the current which the part will use when there is no VCC (i.e. it will pull this small amount of current from the input/output pin when there is no VCC)? Or is that the maximum amount of current you can have at one of the pins when the is no...
    on Jun 24, 2011
  • Forum Post: Fw: Question on SN74AUP3G17 in RSE(QFN) footprint

    Massimo Ferracini Massimo Ferracini
    Hello, I have just tested a new DLP board featuring some SN74AUP3G17 parts. We selected the RSE fooprint, and following component datasheet we designed the net connections: Unfortunatelly, after board testing, I've found that input/output pins are inverted: e.g., channel 1 input is at pin...
    on Jul 11, 2011
  • Forum Post: I2c translator/buffer

    Faraz Firoozabadi Faraz Firoozabadi
    Hello, Can PCA9306YZTR be used for level shifting and also i2c buffer? Also is there any problem to use ESD protection for I2c lines? will it interfere with I2c operation? thanks
    on Sep 1, 2011
  • Forum Post: SN74LVC2244A Supply voltage

    Sakthi Kumar Sakthi Kumar
    Does TI plan to support 1.5V supply voltage for SN74LVC2244A? As of now it is rated from 1.65V.
    on Nov 23, 2011
  • Forum Post: Bus width resizing 16Bit to 8Bit

    Sebastian Kruber Sebastian Kruber
    Dear TI-Team, for our application we need to connect a 16Bit wide camera port (YCbCr) to a 8Bit wide interface (OMAP). What logic can you recommend to serialize the 16Bit data to 2x8Bit data? Regards, Sebastian
    on Apr 2, 2012
  • Forum Post: 5V Tolerant Input 3.3V Buffer, with shared footprint between Mil temp and Commercial Temp

    AndrewKMak AndrewKMak
    Hi, I am wondering if Ti have a (Single, Quad, Octal, etc) buffer that supports: 1) 5V Tolerant Input 3.3V output 2) Common footprint between Mil temp and Commercial Temp Or two parts that share the same footprint, so there is an upgrade path from commercial to military temp. Thank you! ...
    on May 1, 2012
  • Forum Post: SN74LVC244A Question about "Continuous output current"?

    Jean Decuigniere Jean Decuigniere
    Hi all, I would like to use the buffer SN74LVC244A and I see in the datasheet that the Continous output current is (+/- 50 mA). But I don't know if it's +/- 50 mA per pin or +/- 50 mA for the 8 pins total? Best regards, Jean Decuigniere.
    on Jul 23, 2012
  • Forum Post: SN74LVC1G17 logic buffer: can it drive a long PCB track with 75Ohm impedance parallel terminated by 75Ohm resistor at the end?

    Liang Zhou1 Liang Zhou1
    Hi: I need to select a buffer for a 3.3V logic sigal from CPLD. The signal is a few MHz can have to travel 3 feet long of PCB track. If the pcb track impedance is 75Ohm, and I use 75Ohm parallel termination. Then the current consumption is 3.3V/75Ohm=44mA. But the SN74LVC1G17 output is 24mA. I...
    on Oct 13, 2012
  • Forum Post: SN74AVC16374ZQL Pinout

    Andy Goulbourne Andy Goulbourne
    Hi, just a quick one Is the ZQL pinout for the 74AVC374 the same as the GQL pinout? The datasheet lists the pinout for the GQL (page 2), but only the ZQL is available for purchase. Thanks in advance
    on Mar 8, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use