I'm designing the 420M band system using CC1120. And modulation type is 2GFSK.
I would like to know which register should be adjusted for output power calibration.
Is it only PA_CFG2?
Please advise.
Thank you and regards,
Tatsuya.
Yes, it is PA_CFG2.PA_POWER_RAMP that is used to set the output power.
--PS. Thank you for clicking Verify Answer if this answered your question!
Thank you for quick reply.
Does the PA_CFG0 NOT influence for power setting excepting ASK/OOK?
Tatsuya
PA_CFG0 is only used for OOK/ ASK.