• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Hardware & Tools Forum » CC1190 + CC1101 Ref Design SAW filter question
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

CC1190 + CC1101 Ref Design SAW filter question

This question is answered
RF
Posted by RF
on Feb 25 2010 11:02 AM
Intellectual930 points

Hi,

I have seen in the Preliminary CC1101 + CC1190 Ref Design that was posted in this forum that there is a SAW filter between the transceiver and the front-end. I have not been able to find any information about the purpose of this filter. I assume that it is to reduce spurious outputs from the CC1101 to aid in passing FCC requirements but are there any details available about the issue? Like what frequencies are a problem for FCC? Or is it mainly to prevent interference from pager and cell phone base stations that are nearby the 915MHz band?

Thanks,

Russ

 

cc1101 CC1190 reference design saw filter preliminary
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Sverre
    Posted by Sverre
    on Feb 25 2010 12:08 PM
    Verified Answer
    Verified by RF
    Genius14150 points

    Russ,

    The reference design you refer is indeed preliminary and does not come with any documentation. When the reference design is put on the web there will also be a design note with electrical parameters.

    As for the SAW filter: This is included in the design to attenuate CC1101 harmonics so that the harmonics emitted by CC1190 (which also includes harmonics generated by CC1190 itself) are below the FCC 15.247 requirements. Please note that the 3rd, 4th, 5th, 6th, 8th, 9th harmonics all fall in restricted bands were the limit is -41.2 dBm. The main concern will be the 3rd, and if the output power is +27 dBm, the harmonic needs to be 68 dB down. This mandates for a SAW filter. Please note that I assume no duty cycle relaxation factor. That is, the transmission lasts for more than 100 ms. [Note on relaxation factor:  The spurious emission limit is -41.2 dBm inside the restricted bands, but FCC allows for up to 20 dB higher peak emission if duty cycling is being used. The maximum TX on time must be less than 100 ms to get a benefit from this rule. The relaxation factor is 20*log(TX_ON_TIME/100 ms)]

    An added benefit of the SAW filter is the improved out-of-band blocking performance.

    CC1190 reference design FCC saw filter cc1101-cc1190 fcc 15.247
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • RF
    Posted by RF
    on Feb 25 2010 12:17 PM
    Intellectual930 points

    Hi Sverre,

    Thanks for the quick and detailed response. That is exactly the information I was looking for.

    Russ

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kentxu
    Posted by Kentxu
    on Apr 18 2010 14:46 PM
    Intellectual300 points

    Hello,

    I have seen in swra319 "CC1190 FAQ";

    Q: What output power can I expect when using the CC1190 combo boards (EMKs)?
    A: The CC1101-CC1190- 915 EMK combo board can deliver up to +26dBm and still
    meet FCC part 15.247 regulations. The CC1101-CC1190 868 EMK combo board can
    deliver up to +20dBm and still meet ETSI EN300 220 Regulations.

    I assume the limit of +20dBm@868 is due to more strict spurious limitations in ETSI. Is there any way to use the full +27dBm at 868?

    Would it be possible with duty cycling as per FCC?

    Thanks, Ken

    CC1101-CC1190 868
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sverre
    Posted by Sverre
    on May 06 2010 06:49 AM
    Genius14150 points

    Ken,

    Sorry for slow response on this.

    The CC1101-CC1190 can do +20 dBm in Europe. The limitation is the modulation bandwidth requirements under EN 300 220 (BW between -36 dBm points in the output spectrum). For +27 dBm at 868 MHz you need to use a transceiver with less phase noise

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kentxu
    Posted by Kentxu
    on May 11 2010 02:05 AM
    Intellectual300 points

    Hello Sverre,

    Thank you for the reply. Would +27dBm be possible with the CC1020+CC1190?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Aleks46713
    Posted by Aleks46713
    on May 11 2010 02:55 AM
    Prodigy60 points

    Hello.

    So even if SAW filter is used in CC1101+CC1190, it is still impossible to pass European limitations ? (assuming 0.5W ERP and following CC1101+CC1190 reference design).

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sverre
    Posted by Sverre
    on May 11 2010 03:27 AM
    Genius14150 points

    +27 dBm will be possible with CC1020 + CC1190. Only looked at low data rates (4.8 kbps), but in this case there will be a significant margin to the modulation bandwidth requirements.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sverre
    Posted by Sverre
    on May 11 2010 03:51 AM
    Genius14150 points

    The maximum output power is limited by the modulation bandwidth requirements

    • At the bandedges the power needs to be less than -30 dBm measured in 1 kHz RBW
    • At the bandedges +/- 200 kHz the power needs to be less than -36 dBm measured in 1 kHz RBW
    • At the bandedges +/- 400 kHz the power needs to be less than -36 dBm measured in 10 kHz RBW
    • At the bandedges +/- 1 MHz the power needs to be less than -36 dBm measured in 100 kHz RBW

    A SAW filter will not improve on modulation bandwidth as it is too close to the carrier. A SAW filter is still needed though, but this is to attenuate spurs both below and above the carrier.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kentxu
    Posted by Kentxu
    on May 11 2010 04:35 AM
    Intellectual300 points

    Hello Sverre,

    Thanks for the clarification of the requirements. The CC1190 data sheet shows a connection between the CC1020 and CC1190 with some passives and a SAW. Is there a more detailed schematic showing component values, or even better a CC1020+CC1190 Ref Design?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ender
    Posted by Ender
    on May 11 2010 06:25 AM
    Prodigy120 points

    Hello Sverre,

    Apparently, C1020+CC1190 could pass European limitations but your main concern is about the modulation bandwidth requirements.

    However, for what I understand from ETSI EN 300-220, the modulation bandwidth requirement applies only to  equipment with a bandwidth above 200kHz. Otherwhise (eg equipement with a bandwidth below 200kHz), it is necessary to be compliant with the adjacent channel power requirements .   

    So, would it still be possible to meet ETSI EN 300-220 by using a channel spacing of 25kHz and 27dBm output power.

    Thank you

    cc1101 cc1020 CC1190
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sverre
    Posted by Sverre
    on May 11 2010 06:37 AM
    Genius14150 points

    To answer your question regarding a CC1020+CC1190 reference design. We do not have such a design, but once the CC1101+CC1190 design is released you can simply change CC1101+balun with CC1020+output/input match.  

    In Europe you can transmit at +27 dBm in the 869.4 to 869.65 MHz range. The whole band may be used as 1 wideband channel so no need to comply with ACP requirements. BTW: in the new ETSI EN 300 220 narrowband is now =<25 kHz.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ender
    Posted by Ender
    on May 11 2010 07:31 AM
    Prodigy120 points

    Thank you for your quick answer.

    Actually, using one wideband channel is not an option for us: we need to use sub-bands in the 869.4 - 869.65 MHZ range (25kHz channel spacing) and I guess ACP applies.

    In fact, that is not my main concern and I have a few more questions. We made some tests with the CC1190-868MHz reference design and the output power is close to 20dBm. In the same time, we tried the CC1190-915MHz reference design, but with a transceiver CC1020 configured at 869.625MHz. The power available at the PA output is close to 27dBm but I guess that the output matching is quite bad.....

    So, I have two questions after that:

    - How is performed the 20dBm limitation in the CC1190-868MHz reference design??? In fact, there is just a few changes of values between the 915 and 868MHz reference designs, so I am quite lost with that!

    - Is it recommanded to use the 915MHz reference design with a transceiver configured at 869MHz? Or is it possible to improve the current consumption by slightly changing the reference design?

    Finally, in order to understand the matching network beetween the CC1190 and the antenna, one thing missing in the CC1190 datasheet is the PA load impedance and the LNA input impedance (VS frequency). Do you have these informations ?

    Do not hesitate to ask me more informations if it is not really clear.....

    Thank you

    cc1101 cc1020 CC1190
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Aleks46713
    Posted by Aleks46713
    on May 11 2010 08:04 AM
    Prodigy60 points

    Thanks, Sverre. I really forgot to say, that I am going to occupy whole 869.40 - 869.65 band, using only one channel. It's clear now.

     

    Ender,  you can see this topic: http://e2e.ti.com/support/low_power_rf/f/155/p/35307/125067.aspx

    There are reference designs for CC1101+CC1190, so you dont need to know impedance of the CC1190 input and output. The topology, BOM and everything is given there, so we need just copy all stuff between CC1190 and SMA connector. :)

     

    P.S.  sorry if I am saying something wrong.I am just amateur. :)

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ender
    Posted by Ender
    on May 18 2010 02:32 AM
    Prodigy120 points

    Hello Aleks,

    Sorry for slow response on this.

    I already looked at CC1101+CC1190 reference design, but apparently, it can't pass EN 300-220 for our application (sub-bands of 25kHz in the 869.4MHz - 869.65MHZ range and 27dBm output power). That is why I am trying to get more informations.

    Thank you

    cc1101 cc1020 CC1190
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Shawn Hintermeyer
    Posted by Shawn Hintermeyer
    on May 05 2011 16:50 PM
    Prodigy30 points

    Hi Ender, I saw that you are having trouble getting passed some the standards with that RF Filter. It can be tough so you may want to check the impedance of what you are going for to see if there is another kind of rf filter you can use. TI has some incredible ones but if you need anything custom done that might be another ball of wax entirely check out some other rf filter  references to see if you can get some better specs http://www.oscilent.com/catalog/Category/rf_saw_filter.htm


    saw filter rf filter
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use