Hello.
In SmartRF Studio for CC1101 at 433 MHz, if I select, among the preferred settings, 100 kBaud sensitivity optimized, I obtain:
- Datarate about 100 kBaud
- Frequency deviation 47.6 kHz
- RX filter bandwidth 325 kHz.
According to Carson's rule, the signal bandwidth is about 2(Delta-f + fm), where Delta-f is the frequency deviation and fm is the maximum frequency of the signal. This gives 2(47.6 + 100) = 295.2 kHz.
The CC1101 datasheet (page 35, chapter 13) states that "For best performance, the channel filter bandwidth should be selected so that the signal bandwidth occupies at most 80% of the channel filter bandwidth".
80% of 325 kHz is 260 kHz, so it appears that the bandwidth of the signal is wider than 80% of the channel filter bandwidth.
Moreover, if I select, among the preferred settings, 250 kBaud sensitivity optimized, I obtain:
- Datarate about 250 kBaud
- Frequency deviation about 127 kHz
- RX filter bandwidth 541.67 kHz.
Again, according to Carson's rule, the signal bandwidth is 2(250 + 127) = 754 kHz, far greater than 541.67 kHz!
What's wrong with that? What am I missing? (Sorry, but I'm not an RF expert...)
Another problem I am not sure to understand is about channel spacing: SmartRF Studio appears to leave channel spacing at 200 kHz, disregarding all other settings. But if the receiver filter bandwidth is set to 541 kHz, does it mean it takes almost 3 channels? So, in a multichannel environment, I should only select, say, channels 0, 3, 6, and so on, should I?
The last question: when I set the RF frequency, am I setting the center frequency or the base one? In other words, if I set, say, 432.9 MHz with a receiver filter bandwidth of 200 kHz, will the bandwidth of the receiving filter go from 432.8 to 433.0 MHz or from 432.9 to 433.1 MHz?
Thanks,
Stefano