Hi,
In the CC2430 datasheet, there is the input voltage high and low. Each one is given in a range (min, max and typical). And the output voltage? In many components, for the input there is a trigger voltage (0 beyond the trigger, 1 above it), and for the output there is a range (logic "1" between A and B anc logic "0" between C and D), Does the output voltage range is the same as the input? I need to connect a FT232R to a CC2430EM and i need to check if the range matches...
Thanks,