Hi,
I have CC2510DK-MINI. During the test mode PM2 and PM3 I see that modules consume ~24 uA.
I read your appnotes about power saving. Also I used your example.
Why modules consume so much?
I checked Pull-Up resistor. In both modules Pull-Up res on P0_2 pin = 3.61-9 M. Is this normal?? Or, I bought a faulty modules in estore.ti ?
Rev: 1.0
SN: 0000 087C
SN: 0000 0879
Hi Andrey,
According to CC2510 datasheet, the internal pull-up/down typical resistors' value should be 20KOhm.
So, there are 3 options:
Br,
Igor
http://www.youtube.com/watch?v=rxXCXxB-XBE
With these modules, something is wrong. Pull-Up/ Pull-Down res on P0.2 not work.