GPIO3 on the CC1125 is experiencing a weird toggle when switching from SLEEP mode to RX mode when running Wake-On-Radio (WOR). I am configure GPIO3_CFG as 0x14 for MARC state wake up. The problem is that when in SLEEP mode, GPIO3 is hardwired to 1 and then when the radio switches to RX mode and the GPIO3 pin goes to 0 which fires an interrupt on my MCU. I thought that setting the GPIO3_INV bit to 1 would fix this because the pin would be hardwired to 0 in SLEEP mode, but this inverts the entire signal so that the pin now goes to 1 when the radio enters RX mode, which still triggers an interrupt. I need some way to use the GPIO3 pin for MARC state wake up in WOR mode, any suggestions would be appreciated.