hi!
I have been using the code size limited version of IAR for 8051-version 8.30 to start development for a project using the CC111/CC1110. I m using CC debugger 2540 to load the code. It worked correctly until now.
But now, the red ligth is always on and when I try to debug it I see that :
"Thu Apr 17, 2014 17:14:51: Fatal error: Failed to identify device. Check connections and/or reset hardware Session aborted!"
Do you have any suggestions??