Hello,
I was wondering what are the certifications for CC2510dk. Is it certified for worldwide use?
If it is certified and one were to use the reference design as is, can the certifications be inherited?
Ben.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I was wondering what are the certifications for CC2510dk. Is it certified for worldwide use?
If it is certified and one were to use the reference design as is, can the certifications be inherited?
Ben.
CC2510EM (2.4 GHz) has been certified at an accredited external test house; regulations EN300 328 (Europe) and FCC 15.247 (US). Certification cannot be "inherited" and you need to certify your end application.
Best advice: follow the reference design
Ben,
To add to what Sverre said, the only way to inherit a certification is if you use one of our third party modules. They have obtained modular certification and provide fully tested modules for customer to put into there products.
If you comply with all of the module companies requirements (layout, settings, software) then and only then can you inherit their certification.
Regards,
/TA