• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Hardware & Tools Forum » All Tags » #CC1120
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
#CC1120
  • # CC1110 #CC1111 design SPI
  • # CC1110 #CC1111 design SPI #CC1101 TX Package
  • #cc1120 #cc1110
  • #CC1120 sensitivity
  • 169 MHz
  • Application note
  • cc1120
  • msp430
  • Sniff mode
  • STM32
  • Wireless M-Bus
  • wmbus
Related Posts
  • Forum Post: RSSI calculation

    Mirco Pizzichini Mirco Pizzichini
    Hi I've a problem with CC1120 RSSI register. I can see from User Guide that I can read two register (RSSI1 and RSSI0) for a 12 bits number, or using 8 bits from RSSI1, but result is different. Maybe I've to change other registers/settings to change RSSI resolution? Code I use is: cc112xSpiReadReg...
    on Jul 30, 2012
  • Forum Post: CC1120 sync detect on carrier from second CC1120

    Mark Green Mark Green
    Hi, I have a legacy design which I am changing from CC1020 to the CC1120. The system consists of a wireless master (Panel) which communicates to several wireless slaves (Devices). Messages can be exchanged as follows: Panel can talk to Devices; Devices can talk to the Panel; Devices not allowed...
    on Aug 9, 2012
  • Forum Post: Design note - CC112x RX Sniff Mode (TBD)

    Enok Enok
    Hi Team, I see following description "DNxxx CC112x RX Sniff Mode (TBD)" on the design note( TrxEB RF PER Test Software Examples User's Guide (Rev. A)) http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=swru296a&fileType=pdf Do we have a plan to release it yet...
    on Aug 30, 2012
  • Forum Post: CC1120 LNA addition

    Seishin Seishin
    Hi All, I achieve a receiver sensitivity of -125dBm with the current model using CC1020 and LNA.(400MHz band in Japan) Are more than -125dBm possible only by CC1120 reference design? When it is impossible, is the improvement possible by external LNA addition? Best Regards, Seishin
    on Sep 10, 2012
  • Forum Post: CC1120 T/R Switch

    Seishin Seishin
    Hi All, I design the circuit to a current product using CC1020 and T/R RF Switch.(400MHz Band in Japan) I think about a design in CC1120, but do not have any problem using external T/R RF Switch like CC1020? Best Regards, Seishin
    on Sep 10, 2012
  • Forum Post: CC1120EM Reference Design R321

    Seishin Seishin
    Hi All, Now we are designing our board using CC1120, which frequency band is fixed 420 – 470MHz. The attached schematic (CC1120EM-420-470-RD) is what we are referring for this design. Then we are confused by the description “do not mount R321” for using both TCXO and XTAL...
    on Sep 18, 2012
  • Forum Post: RE: CC1120 solution with MCU (MSP430)

    rhso rh rhso rh
    hi Martin, I am currently using TrxEB based on msp430 and an RF module based on CC1120 . I'd like to use the STM32 microprocessor instead of my current msp430 . Is is possible to change the MCU in Smart Rf to a CC1120 SPI connection . If not, why is it not possible? thank you. Cordially...
    on Sep 18, 2012
  • Forum Post: CC1120 Register Setting

    Seishin Seishin
    Hi, Are there any rules in order of the set of registers in CC1120? For example, FS_CFG register must be written in after setting up FREQ2-FREQ0 registers. Best regards, Seishin
    on Nov 14, 2012
  • Forum Post: CC1120EM with A TI ARM eval board

    P.Mutasingwa P.Mutasingwa
    I would like to use the CC1120EM transceiver board with one of the TI ARM processors (Cortex-M Cortex-A or Cortex R). Is there any existing eval board for any of the ARM processors that is compatible with the CC1120EM transceiver board ? I want to spend a minimum amount of $$ and would like to skip...
    on Nov 22, 2012
  • Forum Post: CC1120 About FS_SPARE register

    Seishin Seishin
    Hello, Now, we are evaluating the prototype board using the CC1120.(429MHz) There is a question about a setup of FS_SPARE Register. In a user's guide, this register has description of "For test purposes only". When this FS_SPARE register is not set, it becomes the following. ...
    on Nov 23, 2012
  • Forum Post: CC1120 Output Power Step Size

    Seishin Seishin
    Hello, I would like to adjust the output power in smaller step size.(Less than 0.4dB) Please let me know if there are any methods. (Correspondence to the unevenness at the time of the mass production) Best regards, Seishin
    on Nov 23, 2012
  • Forum Post: CC1121 RX/TX packets

    Jasdin Huang Jasdin Huang
    Hi sir We can transmit/receive packets by our board now. But we have some questions. Please help us to clarify it. Thanks ~ 1. If MCU does not read out data from RX FIFO in time, is it possible to have two or more packets in the RX FIFO? If yes, how can we distinguish different packets? 2. Is it possible...
    on Dec 19, 2012
  • Forum Post: CC1120 RF Frequency drift

    Seishin Seishin
    Hi, I am evaluating the CC1120DK now. After issuing the SCAL command, the frequency seems to do the drift by about 5ppm.(in 1 minute at room temperature) There are the contents of the 『1 VCO Calibration』 in the CC112x/CC1175 ERRATA NOTE. Does this workaround is implemented in the SmartRF Studio...
    on Dec 12, 2012
  • Forum Post: Wireless M-Bus and CC1120 in 169 MHz, Is it posible?

    Maykel Alonso Maykel Alonso
    Hi All, I have been reading about that, and also i have the CC1120 eval modules with an MSP430. The CC1120 it works in 169 MHz, and i could send messages from one to other device. The problem it is to configure to work with other devices over the wireless m-bus standard, I try to configure the registers...
    on Sep 24, 2012
  • Forum Post: About CC1120EMK868-915 and 955

    Hirokatsu Hashino Hirokatsu Hashino
    Dear expert I have a plan to develop the board in ARIB STD-T108 . However, Japanese TI says that he can not sell devices because he can not support me. I am going to push forward development progressively. As the first step, I intend to collect configuration parameters that meet the ARIB STD-T108 with...
    on Jan 29, 2013
  • Forum Post: CC1125 RSSI

    johnson Zhang1 johnson Zhang1
    Hi, I have met a problem about CC1125 RSSI, details as follows: 1,The configuration is the sames as the example of Smart RF studio; 2, I can calebrate the RSSI successfully, and the RSSI value is correct when injecting a RF signal above -127dBm. But the value will be a random data such as -128dBm...
    on Mar 18, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use