• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Hardware & Tools Forum » All Tags » cc1101
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
cc1101
  • 433 Mhz
  • 6LoWPAN
  • 868 MHz
  • 868 Mhz range
  • Antenna
  • antenna selection
  • Balun
  • C1101
  • CC debugger
  • CC1000
  • cc1020
  • CC1100
  • CC110L
  • cc1110
  • CC1111
  • cc1120
  • CC1125
  • CC1190
  • CC11xx
  • CC2500
  • CC2500 CC1101 RF tranceiver
  • CC430
  • Chipcon
  • CRYSTAL
  • current consumption
Related Posts
  • Forum Post: Re: using USART in SPI mode to talk with CC2500

    RF4ALL RF4ALL
    Hi, I believe the SimpliciTI port-init code should then be corrected accordingly, to ensure that the CSn pin (P4.2) is indeed GPIO (that is; not peripheral controlled), no matter what prior code events/instructions have occurred: #define MRFI_SPI_CONFIG_PORT() st( P4SEL = (P4SEL & ~BV(__mrfi_SPI_CSN_GPIO_BIT_...
    on Aug 21, 2008
  • Forum Post: Synchronize clocks with CC1101

    Sam4447 Sam4447
    Hello, I have the following idea, but I am not really sure, if it can work as I imagine: we have one transmitter and several receivers. The goal would be to have syncronized timers/counters running on all receivers. Reading the FREQEST register, I find out how much the carrier frequencys differ from...
    on Aug 28, 2008
  • Forum Post: Re: SmartRF04EB

    Jake Salmi Jake Salmi
    Take a look at the smartRF04EB schematic. You will find that the control signals for the EM boards (CC1100 and others all share common connector and pin-out) are available on P1 and P2 connectors. You'll want to jumper over from your MSP430 board to the CSn, SCLK, SI, SO pins on the EM connectors...
    on Sep 11, 2008
  • Forum Post: Re: AGC_FREEZE ; freeze automatic gain control settings ?

    Sverre Sverre
    Try the following: Read back register AGCTEST (address 0x2B) when you receive the first packet. Write AGCCTRL0.AGC_FREEZE = 3 and then write the gain setting back to AGCTEST.
    on Sep 18, 2008
  • Forum Post: Re: sensitivity as function of preamble and sync word

    Sverre Sverre
    The preamble, which ideally is a 0-1 sequence, is used to set up the correct gain in the AGC, sets up the data deciscion slicing level, and does bit synchronization. If the preamble is too short there is not sufficient time for the RX path to be set up correctly before the real data starts coming in...
    on Oct 10, 2008
  • Forum Post: Re: On-Off Keying transmission using CC1101

    esy esy
    Welcome to the forum, 1132511! You will need to make sure PATABLE[0] and PATABLE[1] values for the OOK levels are properly set. See e.g. this FAQ entry (skip step e, f, and g, which are for achieving serial, asynchronous transparent mode instead of the "normal" packet mode that you are using...
    on Nov 4, 2008
  • Forum Post: Re: On-Off Keying transmission using CC1101

    Sverre Sverre
    The register settings you get from SmartRF Studio are optimized for FSK/MSK and not OOK/ASK. Please refer to design note DN022 as this note tells you what registers to change when going from FSK to OOK and also a gives guidelines on how to find the optimum register settings for the AGC
    on Nov 6, 2008
  • Forum Post: Re: touch sensor capabilities by software SoC cc1110-cc2510

    Kjetil Kjetil
    Dima, Please have a look at the following application note for the MSP430. http://focus.ti.com/general/docs/techdocsabstract.tsp?abstractName=slaa379 Do not know anyone that has done this with the SoC. One option could be a MSP+CC1101 or CC2500 solution if the SoC implentation gets rough. Rgds...
    on Nov 12, 2008
  • Forum Post: Re: CC1110 Balun

    Richard Wallace Richard Wallace
    Hi Ron, We have been working with Johanson to adapt a chip filter-balun matched to the CC11xx family. We are on the verge of releasing this as a standard reference design. The part number for this balun from Johanson is P/N 0896BM15A0001. We are seeing very good performance with this filter-balun part...
    on Nov 12, 2008
  • Forum Post: Re: CC1110 Balun

    Richard Wallace Richard Wallace
    Hi, This is not fully released yet from Johanson. The filter balun is matched to the CC1101 and the single ended port is 50 ohm. This will go into series production in Jan 2009. Please contact Ian Johnson at Johanson Technologies: his email is ijohnson@johansontechnology.com Regards, Richard...
    on Nov 13, 2008
  • Forum Post: When I read RSSI value continually, C1101 will crash.

    KevinLee KevinLee
    A function that I would like to read RSSI several times. But when TAG in RF transmit phase and syn chars are the same, then CC1101 crashed. How do I solve this problem?
    on Nov 21, 2008
  • Forum Post: Re: CC1110 and 868 Mhz range

    Richard Wallace Richard Wallace
    Hi, Enclosed are some test results I have acheived when performing range tests with the CC1110/01. With a data rate setting of 250kbps, 0dBm output power, 1.3m above ground, PER:<1%, Nearson dipole antenna; we have recorded 230m_average (690 feet). Best regards, Richard.
    on Dec 19, 2008
  • Forum Post: Re: A problem with CC

    komal komal
    1132511 s hardware, I'm using two MSP430 FG4618/F2013 Experimenter Boards, and two CC1101EMK 434 MHz chips. Hi all, I have the same hardware as above and the simpliciti software. When I run my program using two CC2500 chips it works fine. Then I used CC1101EM 434 MHz chips, without changing the...
    on Feb 5, 2009
  • Forum Post: Re: CC1101 and CC1100 are really compatible?????

    Sverre Sverre
    CC1100 and CC1101 are compatible. Not sure what the input power level (or output power and distance between the units) is in your case, but there are two extremes you should check out: is this a saturation issue (if the units are close)? Try with a lower output power level. is this a sensitivity...
    on Apr 24, 2009
  • Forum Post: Register values for CC1101 in ASK mode

    Ted DEM Ted DEM
    Hi. Please can anyone send me all registers value that we need to put in the CC1101 (RX and TX componants) in order to communicate with two CC1101 componants in ASK mode. I program the CC1101 with an MCU. I try it for several weeks and I am depressed. So, do I need to send a commande strobe after programming...
    on Apr 26, 2009
  • Forum Post: Re: Symmetric CC1101 Matching

    Richard Wallace Richard Wallace
    Hi Fabian, When the tracks and component placement are not symmetrical the output power will decrease and the harmonics will increase due to an inbalance on the PA. More info in DN017. If you have no choice to lay out the components as you suggested, then your layout suggestion will help. Try to maintain...
    on Apr 27, 2009
  • Forum Post: Re: CC1101 range question

    Richard Wallace Richard Wallace
    Hi Z, Good comments, I both agree and disagree at the same time :) The distance of 3km (LOS) is practical but if this has to be guaranteed then the environment parameters will have to be reviewed thoroughly. Totally agree that the antenna choice and height above ground has a huge part to determine...
    on Apr 29, 2009
  • Forum Post: Re: CC1101 Transmission Problem

    M M
    There might be many reasons why your system is not working, so let's start with the basics: - First, did you verify that you can send and transmit packets from one board to another using SmartRF Studio and two evaluation boards? - Read the two documents referred to above carefully. - Starting with...
    on May 14, 2009
  • Forum Post: CC1020 compatibility with CC1100 (CC1101)

    mark tucker mark tucker
    We use the CC1100 (soon changing over to CC1101) in a 915 MHz transceiver module that we produce. We want to modify this transceiver for narrow-band data transmission at 868 MHz. The CC1020 looks like the appropriate chip to use given its low phase noise performance. How much - if any - of our code developed...
    on May 19, 2009
  • Forum Post: Re: sensitivity as function of preamble and sync word

    Seishin Seishin
    Hi, Our client is experimenting with CC2500, they are testing communication between one End device and two two access points(with same settings but different addresses and placed at well seperated distance). But as and when the End point transmits a signal to access point 1, the access point 2 also...
    on May 26, 2009
  • Forum Post: Re: Does a Linux driver exist for CC1100/CC1101 ?

    BrandonAzbell BrandonAzbell
    saz25 We are about to design a board using the CC1100. I'd like to know whether a Linux driver exists for this device. The CC1100 (and the CC1101) is a transceiver device with a SPI interface to connect to an external host. I'm not aware of any linux driver for this device, but there are...
    on May 27, 2009
  • Forum Post: Re: cc1101 comminication through spi

    Richard Wallace Richard Wallace
    Hi Andreas, Do you have the Smart RF Studio kit available ? If not, I recomend to get a kit then you can connect your DUT to the main board and examine the register settings in the Smart RF Studio software. Excellent platform for debugging. Is it only the SO pin that you are having problems with...
    on Jun 9, 2009
  • Forum Post: Power Amplifier for the CC1101 at 315 MHz

    Jeremy Smith Jeremy Smith
    I am looking for a referance design or recomendations for a PA (Power amplifier) to use withe the CC1101 at 315 MHz. Size and output power are the main concerns. Smallest size with the most power out [:D] I am looking for at least 250mW (75mA at 3.3 Volts). Thanks
    on Jun 9, 2009
  • Forum Post: CC1101 RSSI value

    Parcour Parcour
    Hello, currently I try to read out the rssi value of the cc1101. It works, but the value is only between -20 dBm and - 60 dBm. Values below -60 dBm are not possible because there is no connection anymore. I'm using the MSP430 Experimenter's Board. Do you have an idea? Thanks a lot!
    on Jun 15, 2009
  • Forum Post: Refection of harmonics

    Parcour Parcour
    Hi all, can you explain, why the odd harmonics should be reflected back towards the chip (using CC1101)? Is it because a rect signal consists of these harmonics? SWR168a: Preferably the odd harmonics should be reflected back towards the chip with high real part of the impedance. The current consumption...
    on Jun 9, 2009
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use