All,
The link appears to now be working.
I apologize to all for the inconvenience and appreciate your patience through this process.
Regards,
Jim Noxon
If this post has answered your question, even if not the way you wanted, please indicate so by clicking the Verify Answer button on this post.Please start a new thread if your question is not closely aligned with the original post in this thread as it makes searches more effective.If responding to a post please click the Reply button on the post you are responding to rather than merely defaulting to the bottom post.
Hi Jim,
When do you expect to have a release of the stack with support for the cc1121?
I am currently using V1.1.1 of the simplicti stack with the cc1101 and would like to migrate the stack to use the cc1121 hence the reason I ask the question.
would you have any info that might be helpful for this migration?
Kind regards
T.Hunt
Development Engineer
What's the ETA on SimpliciTi 1.2.0 for CCS?
Thanks,
-r
I cannot compile one of the examples distributed with simplicit 1.2.0 on IAR kickstart : it says too much object cod produced..
Is this a problem of settings of procedure or just couldn't be done.
Robert.
HI,
The free version of IAR only allows you to compile programs that generate 4K or 8K of object code (depending on which processor you are using). You can look into upgrading to a full version of IAR. That's what we did, but it is on the pricey side. CCS is also another option. I believe they allow up to 16K in the free version. Their full version significantly cheaper.
HTH,
Barry
blb HI, The free version of IAR only allows you to compile programs that generate 4K or 8K of object code (depending on which processor you are using). You can look into upgrading to a full version of IAR. That's what we did, but it is on the pricey side. CCS is also another option. I believe they allow up to 16K in the free version. Their full version significantly cheaper. HTH, Barry
Hi,
thanks for response. I agree that buying full version is a cure. But what bothers me that I have a project in IAR based on Simpliciti 1.1.1 and can be compiled without any problems (but on IAR 4.21.8) ...
I believe that version 1.2.0 is not much bigger that 1.1.1 - or am I wrong?
Hi Robert,
Perhaps look at the map file from your 1.1.1 project and see how big the code is. Maybe it's just barely under the limit and simplciTI 1.2.0 has pushed it over. Any differences in the optimization settings?
BR,
Is there any update on the release date for the CCS version of simpliciTI 1.2.0?
As discussed in the first post of this thread, that SimpliciTI support to CC1120 is in progress on Nov,2011.
So, is this support ready now ?
If not, when it is expected to ?