• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Proprietary Software & SimpliciTI Forum » SimpliciTI - Multiple Links in End Devices
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

SimpliciTI - Multiple Links in End Devices

This question is not answered
gchaconr
Posted by gchaconr
on Mar 26 2012 14:12 PM
Intellectual280 points

Hi, I have a question about an application I want to implement.

Using the example that SimpliciTI provides for the eZ430-RF2500 devices, the Simple Peer-to-Peer project works fine.
Now I want to implement something similar with two Listerners, where a board is programmed with the application LinkTo and another two boards with the application LinkListen (all of them with different addresses). Thus, the board with the app LinkTo is linked to the other two boards through different links, such that at every time it decides whom to send a message. Is this possible? If so, can I base my code on the example "Access Point as Data Hub", or those features (frequency agility) are not supported for End Devices?.

Also, I have checked the code for the Access Point from the application "Access Point as Data Hub", and I want something similar but instead of the Access Point being listening for links, I want it to be the one looking for links (ie, similar to what the function LinkTo does in the End Devices). Is that possible?


Note that I don't want to send the same message to all the listeners, such one of the application from SimpliciTI examples does.

Hope someone can help me, thanks.

Regards,
Gustavo.

 

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Fabio Scibilia
    Posted by Fabio Scibilia
    on Apr 06 2012 05:37 AM
    Prodigy30 points

    Hi Gustavo,

    Did you find any reply to your answers? I have a similiar conditions in which one end device must connect to two other nodes and push them messages. The first test I did is to use the Sensor Monitor demo application that you can find in the installation CD of eZ430-RF2500. I deployed two nodes with Access Point (using USB FET debugger) that use LinkListen() to accept connections from peers, and when I run the End device (which invokes link() ), both nodes accept the incoming connection request and start plotting the result. From the end device point of view, I have only one linkId to use and when I send messages over that link, both AP receive and plot the message.

    How can I exactly address one node in the link() phase to make a p2p connection (and not a one to many) ?

    Fabio

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • gchaconr
    Posted by gchaconr
    on Apr 06 2012 10:41 AM
    Intellectual280 points

    Hi Fabio,

    I didn't get any answer for my problem, but what I finally implement is the following:

    I need all three the nodes to be end-devices, one listenTo and two Listeners, such that between the ListenTo there exists a different link for each Listeners. The only way to make it possible was to setting each link at different frequency channel. The transceiver of the Listeners are set to an specific frequency channel, and when the ListenTo wants to link to them or send them messages it has to be in their respective frequency channel.

    To change the frequency channel of the transceiver using SimpliciTI, I found the following code:

      freqEntry_t freq;
      static uint8_t sChannel = 0;

      ......// more code

      freq.logicalChan = sChannel;
      rc = nwk_setChannel(&freq);

    where the variable sChannel is the index of the frequency you are using (I am setting for example sChannel=0, 1, 2, 3, or 4; for five different channels). Also to use the code I wrote you have to modify the file nwk_freq.h and the variable NWK_FREQ_TBL_SIZE (to the number of different channels you want to use).

    I am not sure if this is the optimal way to implement what I need but at least works fine. I hope it works for your needs.

    Gustavo.

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Justin Allen
    Posted by Justin Allen
    on Feb 05 2013 11:38 AM
    Prodigy30 points

    I have only been using SimpliciTI for a couple of weeks, so keep that in mind.  I wanted to answer this question since I needed the answer for the last couple of days and could not find it.  

    You can have multiple links with one end device.  Here is the code I am using to set up two links on an ED. You do not need to switch frequencies.

    /* Listen for link forever... */
    BSP_TURN_OFF_LED1();
    BSP_TURN_ON_LED2();
    while (SMPL_LinkListen(&sInLinkID) != SMPL_SUCCESS)
    {
    BSP_TOGGLE_LED2();
    }

    /* Turning on LED2 to show that we have link*/
    BSP_TURN_ON_LED2();

    /* Try to set outgoing link until success */
    while (SMPL_SUCCESS != SMPL_Link(&sOutLinkID))
    {
    BSP_TOGGLE_LED1();
    }

    /* Turning on LED1 to show that we have out link*/
    BSP_TURN_ON_LED1();

    Once the links are established I just use sInLinkID or sOutLinkID, depending on which device I want to communicate with.  For example, here is the code I am using to forward packets from the InLink device to the OutLink device

    /* turn on RX. default is RX off. */
    SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_RXON, 0 );

    while (1)
    { 
       if( sSemaphore ) /* Packet received that needs forwarding */
       {
           /* Radio IDLE to save power */
          //SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_RXIDLE, 0);
          SMPL_Receive(sInLinkID, radioMsg, &len);
          sSemaphore = 0;

          /* Forward packet to outLink */
          SMPL_Send(sOutLinkID, radioMsg, len);

          /* Turn on RX. default is RX off. */
          SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_RXON, 0);
       } 
    }

    The key is you have to change DNUM_CONNECTIONS in the smpl_config.dat file.  When using the smpl_link example DNUM_CONNECTIONS defaults to 1 and you will not be able to establish multiple links unless you change the value.  

    Your application must keep track of which link ID goes with which device so that the correct messages are sent.  I manage this in my simple test network by establishing the links in a preset order so I know which linkID goes to which device, but you could implement something more sophisticated by using the devices address or some other scheme.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use