5277.SimpliciTI-IAR-1.2.1-Beta-20111012.zip
By decrypting the accompanying SimpliciTI-IAR-1.2.1-Beta(20111012).zip file using the enclosed password you agree with the stated SimpliciTI License Agreement found in the same directory as this file.
In addition, you accept the "Beta" release provides no guarantee of merchantability or compatibility with any future official releases of SimpliciTI by Texas Instruments.
Decryption Code: TISimpliciTI
Regards,
Leo Hendrawan
By looking at the SimpliciTIchangelog.pdf file, this appears to be an older version. 1.1.0. Is that intended?
Hi,
this is a beta release, the documentation is not yet updated. sorry for that
Hello.
I agree with blb (Barry). I downloaded this code and compared it with the current Installer 1.2.0 code I have. There are some critical fixes I asked Jim Noxon to include in the 1.2.0 release which he did. These fixes are not in the code I downloaded from this link. This look like 1.1.1 code to me. It is messed up.
BTW The version bytes in the nwk_globals.c of the 1.2.0 release are incorrect.
lfriedman
Hi guys,
thanks for the input. Basically i was only told to upload this beta version to E2E, and i will check this issue with the original file owner.
One thing for sure is that this beta version contains project files for the new TrxEB board which is (AFAIK) not available in the previous v1.2.0. This also includes then the support of CC1120.
I will get back to you as soon as i got some update from the file owner.
Heheh, still waiting for the CCS version of SimpliciTI 1.2.0 :(
Tim Barr
Multitech Systems Inc
i am too
Hi, Leo
I am wondering when the SimpliciTI official version supporting CC1120 will be released. Do you have a schedule?
Thank you!