Hello,
I am working with cc2531EMK device and ZNP example ( stack 2.3.1).
In the example project I can obtain the ".hex" file to program the bootloader and without erasing necesary memory for this.
I have used this ".hex" file and the bootloader starts when the USB is plugged . I don't want it, I would prefer control the moment to start the bootloader.
Is this possible? if it si possible, how can i do it?
My idea is to implement a new command in ZNP comunication and when the new command arrive start the reprogramation.
Regards
I have tried changing something in code, but without good results.
The changes:
- Delay time in boot : uint32 dlyCnt = 0x100; //0x260000
- I have inserted Boot files in ZNP project (sb_exec.c, sb_exec.h, sb_main.c and sb_main.h) with their paths.
I try to build the project but this mistake appear: Error[Pa037]: function type not callable , usbirqHandler();
I don't understand the reason, can somebody help me?