Hi,
We have been looking at developing a consumer device that uses a Low Power RF SoC solution.
Basically we need some advice on the best low power RF SoC and Development Kit to purchase and whether the SimpliciTI protocol will meet our needs. We also need to know what the best antenna DK is for these chips?
Here is some background on what we are setting out to achieve:
We haven't specified this to the point that we have identified all the chip features required but looking at the TI solutions available they all look packed with features.
We have identified the CC2511fx as a possible candidate, as I believe SimpliciTI supports this although the development documents do not mention this. We did start looking at the new CC2540 low power Bluetooth chip, but I cannot see if there any plans for SimpliciTI to support this chip?
Any advice would be greatly appreciated. TIA.
Regards
NozFX
Richard,
Please see my responses below.
Richard Norris We have been looking at developing a consumer device that uses a Low Power RF SoC solution. Basically we need some advice on the best low power RF SoC and Development Kit to purchase and whether the SimpliciTI protocol will meet our needs. We also need to know what the best antenna DK is for these chips? Here is a recently released antenna DK that you can take a look at. The users guide has additional linkes to other antenna design notes. http://focus.ti.com/docs/toolsw/folders/print/cc-antenna-dk.html?sp_rid_pod1=MjEzOTYzNTA1MjcS1&sp_mid_pod1=3201316 Here is some background on what we are setting out to achieve: We require as low cost a production as achievable given the specification. -- Probably a PCB antenna with a discrete balun if you have the real estate for it. We require a small form factor, low power RF capable solution over the 2.4Ghz range as to support the device Globally (I think 2.4Ghz is the best choice?). -- Globally, 2.4GHz makes the best choice right now, Smaller form factors can require more expensive discretes (i.e. chip balun, chip antenna, etc.). Also, keep in mind that smaller antennas will cause the link budget to take a hit as the antenna aperture is reduced. The solution requires USB to interface with a personal computer system. (Windows based primarily, MAC and Linux would be useful) -- probably a CC2511 as first recommendation. There is also some example USB code for these systems which you can look at here http://focus.ti.com/docs/toolsw/folders/print/cc2511nano_refdes.html and http://www.ti.com/litv/zip/swrc088c. The nano design includes a meandered F PCB antenna with a delay line balun, probably about the least expensive RF path you'll find. We haven’t specified exactly the wireless requirements but basically the solution needs to be able to talk to devices using point to point but using automatic discovery of multiple devices communicating with them in a synchronous fashion (needs to send (Tx) and receive (Rx) alternatively). Basically allow devices to identify multiple clients and then talk to them individually in a ordered fashion. -- SimpliciTI does provide some support for localizing and joining networks. Additional mechanisms can always be adapted in user code as well. The data packet size will be low, but not sure how much at present. -- if less then 50 bytes then SimpliciTI can handle without needing the user to partition the packets, otherwise the user code will need to break down the packets into less than 50 byte chunks. The range of the device needs to be around 15 meters or more, roughly in building environment (possibly outdoor too) but not necessarily between rooms or walls. What is the best antenna to use here? -- Most antennas will handle this distance quite easily especially if there are no walls or floors to penetrate. Note that if the device will be worn close to the body, some adaptions to the antenna may be necessary as the body absorbs 2.4GHz energy quite well. It could also shield significants amount of energy if the paired radio is on the other side of the body. Indoors this may not be much of an issue as reflected energy may reduce these effects. We have never developed a wireless protocol before so are hoping SimpliciTI will offer the fastest and most cost effective solution for this. Is it tailorable enough for use to do multiple device discovery and point to point communication? -- SimpliciTI is fully configurable and is normally distributed as source code so you have full access to tweak what you like at all levels. It can be a great starting point for developing proprietary protocols or simply use it as is. If you are new to RF in general and especially packetized protocol stacks, SimpliciTI can ease the learning curve since it is not as full featured as other standards based stacks like Z-Stack (TI's Zigbee protocol stack). We haven't specified this to the point that we have identified all the chip features required but looking at the TI solutions available they all look packed with features. We have identified the CC2511fx as a possible candidate, as I believe SimpliciTI supports this although the development documents do not mention this. We did start looking at the new CC2540 low power Bluetooth chip, but I cannot see if there any plans for SimpliciTI to support this chip? At this point, SimpliciTI does not support the CC2540 device. SimpliciTI does support the CC2511 part as it is basically the same as the CC2510 part with the USB peripheral included. I haven't actually developed any code with SimpliciTI and the CC2511 USB stack code together so I cannot say the two pieces of software will work together without issues but it should get you significantly closer to your goal than where you are currently. Any advice would be greatly appreciated. TIA. Regards NozFX
Regards,
Jim
If this post has answered your question, even if not the way you wanted, please indicate so by clicking the Verify Answer button on this post.Please start a new thread if your question is not closely aligned with the original post in this thread as it makes searches more effective.If responding to a post please click the Reply button on the post you are responding to rather than merely defaulting to the bottom post.
Hi Jim,
Many thanks for your very prompt, clear and concise response. You have reassurred me that we are looking in the right direction, the links are invaluable. I realise there is a lot we will need to be taking into account in the long term, but I'm hoping to start prototyping promptly to prove the concept first. I didn't want to be miles off the type of SoC we used to do this when we invest in its DK.
It will be interesting to find out whether we can achieve what we need to with SimpliciTI; if we are able to tweak the code though, that may give us the flexibility we may eventually require. I'm hoping to keep the networking simple, although this may not be the case. The concept is peer to peer, no repeaters or routers. Its just the device will need to automatically discover and connect to peers. Basically the devices need to be discoverable, a peer then tries to connect to a discovered peer. As soon as connection established the devices no longer talk to any other devices until communication is finished. Internally we will need to keep track of peers that have already communicated as to ensure reconnection does not happen within a set period of time (kind of cache). I guess to realistically achieve this we will need to come up with some proprietry protocol on-top of SimpliciTI?
Is the development kit for the CC2510/CC2511 the kit to use for this? Will there be SimpliciTI examples included with this DK or is this seperate with the SimpliciTI SDK? Sorry, I guess I should just have a look ;) its just it isn't obvious from looking at the web site.
Many Thanks
Richard [NozFX]
Richard Norris It will be interesting to find out whether we can achieve what we need to with SimpliciTI; if we are able to tweak the code though, that may give us the flexibility we may eventually require. I'm hoping to keep the networking simple, although this may not be the case. The concept is peer to peer, no repeaters or routers. Its just the device will need to automatically discover and connect to peers. Basically the devices need to be discoverable, a peer then tries to connect to a discovered peer. As soon as connection established the devices no longer talk to any other devices until communication is finished. Internally we will need to keep track of peers that have already communicated as to ensure reconnection does not happen within a set period of time (kind of cache). I guess to realistically achieve this we will need to come up with some proprietry protocol on-top of SimpliciTI?
I would say yes, that your application will need to keep track of the associations.
Richard Norris Is the development kit for the CC2510/CC2511 the kit to use for this? Will there be SimpliciTI examples included with this DK or is this seperate with the SimpliciTI SDK? Sorry, I guess I should just have a look ;) its just it isn't obvious from looking at the web site.
Yes, the CC2510-CC2511 DK is supported by SimpliciTI in the IAR port version. There are a number of other kits supported by SimpliciTI as well. Some are SoC type devices with the 8051 microcontroller integrated with the radio, CC2510-CC2511DK, CC1110-CC1111DK, CC2430DK, CC2430ZDK.
There are other platforms that are supported as well by SimpliciTI that use a 2 chip solution, Microcontroller + radio. EXP430FG4618 + CC1100, EXP430FG4618 + CC2500, eZ430-RF2500, SmartRF05EB + MSP430F2618 + CC2520.
Brandon
Hi Brandon,
Thank you for your reply, I appreciate your advice, the lists provided are very helpful.
I've pretty much set my heart of the CC2511 or the CC2500 with a seperate microcontroller. I really want the following features:
The problem I now face is RF compliancy. I've just realised this could be a big headache, so have been investigating if anyone has any pre-built modules that are compliant in Europe and the USA.
I've been looking at 3rd party pre-built RF modules using the CC2500 that are FCC compliant. The problem is I cannot find a suitable microcontroller to work with the CC2500 that has USB support. I like the look of the MSP430 but I cannot find a variation with USB. I could add a third controller but this starts to grow the solution somewhat. Is there such a microcontroller I can use with the CC2500 or is there a pre-built module out there with FCC compliance that uses the CC2511?
Richard
I saw your other post inquirying the same information regarding possible modules. I'm not personally aware of a module provider that uses the CC2511, but LS Research does have a module that incorporates a MSP430F5437 + CC2500. Now this particular MSP430 also does not have USB integrated, but there is an application note with using a TUSB3210 (USB-to-UART) device that could be added to your system.
Thank you for your reply.
I had a gutt feeling this would be the case, and from what I've discovered about compliance, it was never going to be the case.
I'm happy to reside myself using the CC2500, but this now presents a tricky set of issues.
What you have suggested may well be the way to go but it has one problem and possible two:
Is there not another MCU with the equivilent functionality of the CC2511 (8051 based architecture) that I could use with the CC2500 and find a decent enough DK to work with it with them both?
Check out these two links
http://focus.ti.com/docs/toolsw/folders/print/cc2511usb_refdes.html
and
http://focus.ti.com/docs/toolsw/folders/print/cc2511nano_refdes.html
Both are reference designs using the 2511 part. You can download the users guides for both without purchasing them and also the code files associated with each.
SimpliciTI has sample applications that work directly on the first link. You will need to incorporate the USB stack files from the software image that comes with it to enable USB operation as the SimpliciTI sample applications only work the radio. Note that you will want to do your development via a CCDebugger (http://focus.ti.com/docs/toolsw/folders/print/cc-debugger.html)so the USB stack integration can be debugged as well.
As far as FCC qualified, you cannot cross that bridge until you have a unit packaged up as FCC qualification must be done on the final product. Some RF modules claim FCC qualifications but unless they have a detailed specification of how it must be mounted, what enclosures it is qualified to operate within, what antennas can be used and their orientation/location, etc., they are most likely just pre-qualified which is just saying they have done some looking and there are no FCC related issues with a stand alone module; most modules fall into this catagory. The above reference designs should work well for you for development and also get you a long ways towards a final product. The PCB antennas are susceptable to de-tuning from whatever enclosure you wrap them in. Although this will probably help you pass FCC testing as it will reduce power output in general, you will most likely want to re-tune the RF path and antenna once you are ready for production and before you go to FCC testing.
You should note that you don't have to do FCC testing to sell your product (at least you don't have to pay anyone to do it or you can do it yourself). If you don't do FCC testing at all you simply cannot state that it "complies" with FCC regulations. However, nothing can eliminate the fact that your product, if sold in the US, will "be subject to" FCC regulations. The 2.4GHz band may be an unlicensed band but anything operating in it is still subject to work within the defined regulations. If you do sell without any FCC testing, the penalties can be higher if your product is found to violate regulations. As always, its a risk/reward balance that your company must decide how to persue.
H Jim,
Thank you very much again for your clear and concise answers.
I'm now feeling rather excited about proceeding with prototyping this product. The RF regulations were beginning to cast a very big shadow over this whole thing. I can now see as long as we approach this with certification in mind we should be ok. It also helps that TI's kits come with reference designs we can follow which should also help with this. The project itself really doesn't need high power nor does it need a long range, so I think we are going to fall into the lowest category (fingers crossed).
I think the CC2511 is the SoC we want to develop with; the links you have provided are spot on with kicking us off. Looks like we'll be purchasing the kits we need pretty soon.
Just one thing to clarify. I realise the USA have pretty tight regulations governed by FCC. Does the same apply for the UK? I believe what you have been saying applies to UK, as in, we can self certify at our own risk? If we wanted certification, have you any adivce on the most cost effective way to go about this? Can we go direct to the governing bodies or does a third party need to be involved?
Many thanks again for your and your other collegues support on this.
Kind Regards
From my experience, which is limited at best with regard to ETSI and the European theater, it seems that the FCC is somewhat more controlling when it comes to out of band issues whereas ETSI seems more interested in makeing sure you are playing nice within the given band. Note that this is purely an engineers perspective when reading the myriad of paperwork from both agencies. There are companies out there which can help you with these issues and some are also certified for certification (pardon the redundancy) in multiple regions.
You are definitely allowed to certify your own products, at least for the FCC but I assume that ETSI, ARIB, etc have similar lower cost paths. In general, the documentation you provide must show due dilligence in your testing proceedures. In effect the documents are what testifies for you to show compiance. The hard part is knowing what documents to produce and which regulations you must adhere to. Also, some of the regulations can be handled merely by showing that your system doesn't operate in that mode, i.e. your system compies by design. Unfortunately, I cannot tell you where that threshold lies or all of the regulatory documents your product is subject to.
In the end, especially if this is yoru first product in the RF world, you are probably much better off looking into a certification organization that is a bit more rather than less. It can cost some extra but the learning curve here is steep and it may actually save you significantly in the end if you will be making follow on products. Do the research now so it is known before you get to the end of the schedule. Also, some certification organisations can have significant lead time. Another reason to look early.
I've known some small companies (1 or 2 employees) which will build the system in a very pessimistic manner hoping that if there are ever any issues they will pass with ease. Then they deploy this system to both test the market and raise some capital. Once they can firm up the business plan, they optimize the system and push the envelope with respect to the regulations as they can now afford proper certification. This approach is not normally appreaciated by larger companies with significant brand name influence but the spectrum is wide in this regard. It all depends on your organization and what risk they are willing to incur.