Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Hi,
I'm aware of eZ430-RF2500 supports SimpliciTI and SimpliciTI used for Star topology networks.I read it is not possible to implement a mesh network due to lack of memory of MSP430F2274, so it can't support. But I need a mesh sensor network ( something like sensor monitor but instead of star topology it must be mesh network ), actually very small one, something like having 4-5 nodes. Is it possible to implement a small mesh network using eZ430-RF2500 or I have to use another kit ?