Hello,
I have a problem with SmartRF04EB and it's device ids. I reprogrammed the board with my own application and overwrite default factory firmware. Now i'm require it again to use the board with SmartRF studio. I have Silicon Lab's usb debug adapter for MCU what i could use for flash a bootloader firmware to the board. After that, i can upload actual firmware with SmartRF studio or SmartRF flash programmer.
Problem arrives with device id's which are same (0x0050) by default. SmartRF flash programmer have option to flash bootloader and set device id with EC2, but i don't have access to such tool. So, what i'm asking is: Is there any way to modify device id when flashing a bootloader? Should i change some bytes on program's binary file?