After entering PM3 following the DN106 specification, CC1110 never wakes on first external interrup, but always wakes on second interrupt.

The interrupt is set to trigger on P0.1 going high. The port input is low when entering PM3, and no interrupts are pending.

The problem disappears when the prescribed DMA transfer ( DN106) is disabled, but is of course not an acceptable solution