Hi. I am developing an application using CC2530. I designed two 4-layer PCBs, each with an Inverted-F Antenna following DN007.
Testing with basicrf, however, I got very low range, even with Tx power set to 4.5dBm. For my application, I need the transmitter (fixed) and the receiver (mobile) to be able to communicate inside a house.
So I put an SMA connector on the transmitter and plugged a 2dBi antenna. It extended the range a little, but it's not even close to what I need for my application.
Would CC2591 be a solution?
Also, I am planning to use SimpliciTI instead of Z-Stack since it's a fairly simple application. Is SimpliciTI compatible with the range extender? I got mixed informations searching around.
Thanks,