Hi;
I am working on AN082 -- Two-Way Audio Communications using the CC1110 or CC2510 and the TLV320A at 433Mz
I want to use FEC property of CC1110.
Does anyone tried to use FEC/interleaver hardware of CC1110?
Thanks
Just got it to work a few hours ago. The customer was looking for a 'One Way' link, 8 kHz sample rate with compression enabled. Data rate is 250 kbps, using GFSK modulation. I haven't done much testing, but the inital results seem to show an improvement in 'walking performance' as compared with the non FEC implemntation at 100 kbps.
Email me (m-burns@ti.com) for details.
Mike Burns
Hello,
has anybody else experiences with error rate with 100kbps via air without FEC and with 250kbps with FEC ? Which seems to work more reliable?