• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Proprietary Software & SimpliciTI Forum » All Tags » smartRF 04 EB
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
smartRF 04 EB
  • CC1100
  • CC1101
  • cc1110
  • CC1111
  • CC111x
  • CC1120
  • CC2430
  • CC2431
  • CC2500
  • CC2530
  • chronos
  • debugger
  • Firmware
  • IAR
  • IAR compiler
  • IAR SimpliciTI
  • RSSI
  • SimliciTI
  • simliciTI 1.1.0
  • SimplciTI
  • SimpliciTI
  • simpliciti 1.1.1
  • SmartRF Studio
  • UART
  • Wake-On-Radio
Related Posts
  • Forum Post: Re: Hardware Debugger for CC2430/31

    R R R R R R
    Hi anybody used new CC-DEBUGGER . Can it do the same functions that can be done with SmartRF04EB board. I mean Can I use it for running "SmartRF studio on CC2430", "Flash programmer software for CC2430" and " Packet sniffer program on CC2430". Thanks, Ramana
    on Jul 23, 2009
  • Forum Post: Getting my code onto a cc2430 soc

    Gregory Yiannatzis Gregory Yiannatzis
    Hey guys, I am using the cc2430 in my final year project at uni and have no idea how i will send the code to the chip. Is it possible to do it without the use of an evaluation board (SmartFR04EB)?. I will be building my own board with the cc2430 on it and all its peripherals (ie 32MHz crystal,...
    on May 14, 2009
  • Forum Post: SimpliciTI on SmartRF04EB+CC2430EM

    adireddy adireddy
    Hi, I had tried working with "AP_as_Data_Hub" application. I had programmed two CC2430EM+SoC_BB with "CC2430-EndDevice" configuration and another CC2430EM residing on SmartRF04EB with "CC2430-Accesspoint". I followed the steps mentioned in "SimpliciTI-SampleApplications"...
    on Oct 28, 2009
  • Forum Post: SmartRF04EB evaluatian board and device id setup

    flarp flarp
    Hello, I have a problem with SmartRF04EB and it's device ids. I reprogrammed the board with my own application and overwrite default factory firmware. Now i'm require it again to use the board with SmartRF studio. I have Silicon Lab's usb debug adapter for MCU what i could use for flash...
    on Oct 29, 2009
  • Forum Post: SimpliciTI on cc2431

    Justin Lee11919 Justin Lee11919
    I've been trying to run SimpliciTI's example's applications on a cc2431 attached to the SRF04 but haven't got any success to get it to work. I'm able to get the example applications working with the cc2430 attached to the SRF04. Is there anything I am doing wrong. From what I understand...
    on May 13, 2009
  • Forum Post: Need Help with Debugging USB using SmartRF04 EB and CC1111/CC2511

    sam yuk sam yuk
    Hi, Im using IAR Embedded compiler on RS232_to_USB_Dongle using SmartRF04EB and CC1111. I come across this msg when trying to debug: "the stack plug-in failed to set a breakpoint on "main". The Stack window will not be able to display stack contents." Does anyone know how to debug...
    on Mar 27, 2009
  • Forum Post: Data send on CC2430

    Jan T. Jan T.
    Hi, I´m a novice in programing RF and I need to send a one bit from one device to other. I work on SmartRF04EB with CC2430. I wanted try SimpliciTi sample program Peer to peer, but it doesn´t work. In debug, program stops on line " MRFI_ASSERT( CHIPID == MRFI_RADIO_PARTNUM ); /* wrong...
    on Oct 7, 2010
  • Forum Post: Communicating only a specific device CC2430

    nectar nectar
    Hi everyone; I'am trying to build a indoor localization system. I use CC2430ZDK, I use HAL library comes with sample applications. My system basicly consist of 1 coordinator, 1 blind node and several referance nodes. I am not using localization enginee since i need to develop it by myself. ...
    on Apr 17, 2011
  • Forum Post: Compiling a project for programming CC2500EM

    Caleb Davison Caleb Davison
    I am new to this whole area and was wondering how I would go about compiling a project. I have downloaded and installed the IAR Embedded Workbench and am wondering how I create a project and which .c and .h files to add to a project. Also, how do I export to a .hex file so I can load the code onto the...
    on Apr 21, 2011
  • Forum Post: help for simplicit

    jie shan jie shan
    hi i have trouble when testing the " Cascading End Devices " about simpliti. i download program in all of three End Devices and they run normal. but when one of them is alarming,the other two can not hear it unless they moved very close(in 50 mm) . i put a breakpoint in "BSP_ISR_FUNCTION"...
    on Aug 24, 2011
  • Forum Post: rx_peek() not working using simplicti UART driver; uart_intfc.c

    Shreyas Venkatesh Shreyas Venkatesh
    HI, I am using SimplicTi UART driver to program CC2530(uart_intfc.c). I am actually programming it in order to receive data from the PC to the EM. When I use rx_peek() should return the value with number of bytes of data in the buffer. But, when i use in my code the return value is always to 2...
    on Jan 23, 2012
  • Forum Post: CC1120 Output Power Calculation and Smart RF Studio

    Jeffrey Wilczewski Jeffrey Wilczewski
    According to the datasheet for the CC1120 Output_Power = ((PA_POWER_RAMP+1)/2)-18 So for example, for an output power of 10 dBm according to the formula 10 dBm : PA_POWER_RAMP = 55 However, the value generated in SmartRF Studio (1.7.0) shows for 10 dBm TX power PA_POWER_RAMP = 0x34 (52 decimal...
    on Jan 24, 2012
  • Forum Post: CC1111 and CC1101 unable to communicate

    G.M. G.M.
    Dear, I'm try to establishing a communication between CC1101 evalboard and CC1111DK_Dongle board but I'm not able to do that. The registers setting (standard setting of smartRF) of both radio are listed above. Can you help me? Are these settings correctly defined? BR, Giordano...
    on Feb 20, 2012
  • Forum Post: srf04 fatal error: failed to identify device

    Nicola Barbon Nicola Barbon
    Hello, I'm stopped by download and debug error. I've installed iar evaluation 7.60.1 and the last patch 7.60.6. I've downloaded and unpacked SimpliciTI 1.2.0 version and I've installed and connected, via usb, the srf04eb with the last firmware 045 (updated with Smarf RF Studio 7)....
    on Feb 7, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use