• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF ZigBee® Software & IEEE 802.15.4 Forum » can i use I2C in CC2530 ?
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

can i use I2C in CC2530 ?

This question is answered
LAKSHMANAN KUMAR RANGARAJ
Posted by LAKSHMANAN KUMAR RANGARAJ
on Oct 18 2011 03:49 AM
Expert1765 points

Hi TI,

 I am planning to use I2C in CC2530. I understand TI CC2530 dont have the I2c module hardware support.It only support TI CC2533.


So to use I2C in CC2530 ,

GPIO p1.3 and P1.4 pin for I2c master. P1.3 use as a clock (use timer 3 to generate pwm clock for 400khz) and P1.4 for SDA.


Kindly advice .whether i can use the above way to communicate with I2C Slave.if there is anyother way please advice.


Thanks and Regards

Lakshman.

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Igor Sherer
    Posted by Igor Sherer
    on Oct 18 2011 04:00 AM
    Guru21965 points

    Hi Lakshman,

     

    You can implement the communication it the FW level, without using timers.

    Syncronising timer output with data write (read) on P1.4 is a hard work and

    involves constant polling of Timer3 overflow, or interrupt.

    If you need a short access (write/read 10 bytes) to your slave, where this access period

    can be done in a time of ~few dozens of uSeconds you can, and you should, implement

    the I2C inside the code without using timers or interrupts.

    Br,

    Igor

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • LAKSHMANAN KUMAR RANGARAJ
    Posted by LAKSHMANAN KUMAR RANGARAJ
    on Oct 18 2011 04:25 AM
    Expert1765 points

    Hi Igor,

     Thanks for the immediate reply.

    I didnt understand the solution. Can you please throw some light ?

    How can i get the clock for I2C  SCL ???

    I need 400Khz clock whenever i need to send the data . kindly advice.

     

    Thanks and Regards

    Lakshman.

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Igor Sherer
    Posted by Igor Sherer
    on Oct 18 2011 05:04 AM
    Verified Answer
    Verified by LAKSHMANAN KUMAR RANGARAJ
    Guru21965 points

    Hi,

     

    Lets say that you toggling P1.3 (which is the SCL) in the following way (transaction of a single byte through I2C):

    P1.3 = HIGH;
    tmpByte = dataFor_I2C_Slave[SomeIndex]; // Just for the example 

    for( int i=0; i<sizeof(byte)-1; i++ ) {
    P1.3 = P1.3 ^ 0x01; // Toggle P1.3 output
    blockingDelay(WRITE_DELAY); // Delay needed for Slave to detect rising/falling of SCL
    p1.4 = !(!(tmpByte & 0x80)); // Set P1.4 with current MSB in tmpByte
    tmpByte <<=  1;
    blockingDelay(CLOCK_DELAY); // Delay needed for generating a ~400KHz SCL
    }

     

    Please note that it is not an accurate example of how to implement the IC2, the important

    thing here is the blockingDelay() function, where in first call for this function used to provide

    a delay for the slave to capture the falling or rising of the SCL. The second call for this function

    intended for delaying the next setting of P1.3 output to create SCL timing of ~400KHz.

    The blockingDelay() can be implemented in the following way:

    void blockingDelay( uint16 delay )
    {
    while( delay ) {
    delay--;
    asm("NOP"); // Here "NOP" is a single system clock instruction (in case
    // of cc2530 1 system clock = ~31.5nSeconds
    }
    } 

     

    Br,

    Igor

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • LAKSHMANAN KUMAR RANGARAJ
    Posted by LAKSHMANAN KUMAR RANGARAJ
    on Oct 18 2011 05:12 AM
    Expert1765 points

    Hi Igor,

     Thanks for your reply. I got it. So i simulate 400khz by means of delay.

     

    This is what i need. thank you so much.

     

     

    Thanks and Regards

    Lakshman.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Igor Sherer
    Posted by Igor Sherer
    on Oct 18 2011 05:21 AM
    Guru21965 points

    Hi,

     

    Just keep in mind that long blocking delays can harm Z-stack normal behavior.

     

    Br,

    Igor

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Felix Bruckmüller
    Posted by Felix Bruckmüller
    on Oct 21 2011 01:56 AM
    Intellectual835 points

    There are i2c hal drivers (hal_i2c.c, hal_i2c.h) available in RemoTi Stack for cc2530.

    I use them with Z-Stack to read data from different sensors without problems.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Igor Sherer
    Posted by Igor Sherer
    on Oct 21 2011 02:01 AM
    Guru21965 points

    Hi Felix,

     

    It is a nice thing to know, thank you very much for the information.

    Br,

    Igor

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • huabai shen
    Posted by huabai shen
    on Mar 22 2012 22:39 PM
    Prodigy10 points

    Hi Felix:

      How could I get the REmoTi Stack for cc2530. I found it on TI's website but it need to request.could you send me one .linux_makefile@qq.com

      thanks and best regards.

    huabai

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Felix Bruckmüller
    Posted by Felix Bruckmüller
    on Mar 23 2012 01:58 AM
    Intellectual835 points
    i2c.zip

    huabai shen

    Hi Felix:

      How could I get the REmoTi Stack for cc2530. I found it on TI's website but it need to request.could you send me one .linux_makefile@qq.com

      thanks and best regards.

    huabai

    Hi,

    I attach the original files to this post.

    Felix

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • greenja
    Posted by greenja
    on Jul 31 2012 04:28 AM
    Guru11490 points

    I made modifications to the hal_i2c.c in order to read and write to the TI PCA9555 I2C 16 bit Port expander using theCC2540.

    This allows me to read and write to just about any I2C device.  This is for the CC25xx  that do not have i2c in hardware.

    To read I use this function:

      if ( I2C_ReadMultByte(PCA9555_ADDR_WR, InPort0, data1, 2 )  )
    ...

    To write:

    I2C_WriteMultByte(PCA9555_ADDR_WR, PolInvP0, data1, 2);

    The function I wrote for reading is:

    /*********************************************************************
     * @fn      I2C_ReadMultByte
     * @brief   reads data into a buffer
     * @param   address: linear address on part from which to read
     * @param   reg: internal register address on part read from
     * @param   buffer: target array for read characters
     * @param   len: max number of bytes to read
     * @return  void
     */
    uint8 I2C_ReadMultByte( uint8 address, uint8 reg, uint8 *buffer, uint16 len )
    {
      uint16 i = 0;
      uint8 I2C_ERROR = 0;
      uint8 I2C_SUCCESS = 1;

      if (!len)  {
        return(0);
      }

      /* Send START condition */
      if( hali2cStart())
        return I2C_ERROR;

      /* Set direction of transmission */
      // Reset the address bit0 for write
        address &= OCM_WRITE;

      /* Send Address  and get acknowledgement from slave*/
      if ( !hali2cSendByte(address))
        return I2C_ERROR;

      /* Send internal register to read from to */
      if ( !hali2cSendByte(reg))
        return I2C_ERROR;

      /* Send RESTART condition */
      if( hali2cStart())
        return I2C_ERROR;

      /* Set direction of transmission */
      // Reset the address bit0 for read
        address |= OCM_READ;

      /* Send Address  and get acknowledgement from slave*/
      if ( !hali2cSendByte(address))
        return I2C_ERROR;

      /* Read data into buffer */
      // read bytes of data into buffer
      while ( len )
      {
        // SCL may be high. set SCL low. If SDA goes high when input
        // mode is set the slave won't see a STOP
        hali2cClock(0);
        OCM_DATA_HIGH();

        buffer[i] = hali2cReceiveByte();
        // Acknowledgement if not sending last byte
        if (len > 1)
          hali2cWrite(SMB_ACK); // write leaves SCL high

        // increment buffer register
        i++;
        // Decrement the read bytes counter
        len--;
      }

      // condition SDA one more time...
      hali2cClock(0);
      OCM_DATA_HIGH();
      hali2cWrite(SMB_NAK);

      hali2cStop();
      return I2C_SUCCESS;
    }

    For writing:

    /*********************************************************************
     * @fn      I2C_WriteMultByte
     * @brief   reads data into a buffer
     * @param   address: linear address on part from which to read
     * @param   reg: internal register address on part read from
     * @param   buffer: target array for read characters
     * @param   len: max number of bytes to read
     * @return  void
     */
    uint8 I2C_WriteMultByte( uint8 address, uint8 reg, uint8 *buffer, uint16 len )
    {
      uint16 i = 0;
      uint8 I2C_ERROR = 0;
      uint8 I2C_SUCCESS = 1;

      if (!len)  {
        return(0);
      }

      /* Send START condition */
      if( hali2cStart())
        return I2C_ERROR;

      /* Set direction of transmission */
      // Reset the address bit0 for write
        address &= OCM_WRITE;

      /* Send Address  and get acknowledgement from slave*/
      if ( !hali2cSendByte(address))
        return I2C_ERROR;

      /* Send internal register to read from to */
      if ( !hali2cSendByte(reg))
        return I2C_ERROR;

      /* Write data into register */
      // read bytes of data into buffer
      while ( len )
      {
        // SCL may be high. set SCL low. If SDA goes high when input
        // mode is set the slave won't see a STOP
        hali2cClock(0);
        OCM_DATA_HIGH();

        /* Send Address  and get acknowledgement from slave*/
        if ( !hali2cSendByte(buffer[i]))
          return I2C_ERROR;

        // increment buffer register
        i++;
        // Decrement the read bytes counter
        len--;
      }

      hali2cStop();
      return I2C_SUCCESS;
    }

    PCA9555 I/O i2c port expander CC2540 CC2530
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Flor
    Posted by Flor
    on Aug 10 2012 15:42 PM
    Intellectual260 points

    Hi greenja, 

    Thank you for sharing your code. 

    I am trying to interface a magnetometer to the CC2540 via I2C but I am not able to get the ACK from the magnetometer.

    I am using the hal_i2c.c  from RemoTI and NOPs to generate some delays to get a frequency below 100 kHz from the 32MHz system clock but still not working... =(

    I am able to see in the oscilloscope that the master is sending the slave address correctly and the frequency of the clock is around 10kHz. The problem is that I am never getting the ACK back from the slave.  

    I use the hal_i2c.c implementation with the  HAL_I2C_RETRY_CNT to retry 3 times to send the address . I can see all the retries on the oscilloscope and the sequence is like this:

    slave address - start condition -slave address -start condition -slave address ... 

    Is there any additional delay or clock cycle that has to be added after the slave address is sent to give some time for the ACK?

    Any help would be greatly appreciated!!!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • greenja
    Posted by greenja
    on Aug 10 2012 21:13 PM
    Guru11490 points

    Hello Flor,

    What mangnetometer are you using?  I did have some code for the LSM303DL somewhere but I can't remember the specifics on how I got it to work.

    Here are the files that I am currently using to interface the CC2540 to the PCA9555 I/O expander for running a LCD and 7Seg displays. 

    There are slight variations to the Hal_i2c.zip that was originally posted, can't remember exactly what I changed, so I just included the whole file.  I don't think the clock rate section really works.  I think I scoped all the values and there was no change in clock speed.

    4265.Hal_i2c-1.zip

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Flor
    Posted by Flor
    on Aug 11 2012 08:55 AM
    Intellectual260 points

    Hi greenja,

    Thank you very much!! I will give it a try. The magnetometer I am using is the LSM303DLH.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • greenja
    Posted by greenja
    on Aug 11 2012 09:08 AM
    Guru11490 points

    I just llooked over the code. You  obviously have to change the OCM_CLK_PORT, data port and pins to match what you are using.  I think the main problem was with theses three lines:

    #define OCM_ADDRESS  (0x4E)
    #define OCM_READ     (0x01)
    #define OCM_WRITE    (0xFE)
    Your address has to be the write address.  In the case of the LSM303 there are two.
    For the sections I added, you don't have to worry because it doesn't use this, the lines in the hali2cReceive are commented out, so you can read from the compass and the accelerometers.

    hali2cReceive

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use