Hi,
My scenario: after ZC is "full" (21 ZEDs are associated to him, then next one fails) I reboot the ZC, but none of the ZEDs can rejoin.
Looking at the Superframe Specification, before and after:
Before (association success):
association permit subfield of the superframe specification = 1
Router capacity = 1
End device capacity = 1
After (association fail):
association permit subfield of the superframe specification = 0
Router capacity = 0
End device capacity = 0
- I'm using ZStack-CC2530-2.3.1-1.4.0. I was advised to upgrade to 2.5.1, but is it necessary? In ZC, ZR and ZED, or only ZC is enough? I prefer not to, due to time restrains.
- I just moved the ZC and ZR to ZIGBEEPRO. ZEDs are still without the ZIGBEEPRO. I prefer not to change them - will that be a problem?
- I'm trying to figure out how to plat with the number of allowed ZEDs in a ZC.NWK_MAX_DEVICE_LIST in nwk_globals.h doesn't really work.
Thanks.