Low Power RF & Wireless Connectivity
Forums
Announcements
Files
E2E Wiki
Options
Subscribe via RSS
Questions regarding Zigbee libraries,CC2530 ZDK,mini ZDK.
Questions regarding Zigbee libraries,CC2530 ZDK,mini ZDK.
This question is not answered
Posted by
JAGAS EDARA
on
Dec 27 2012 06:37 AM
Intellectual
920
points
Hi All, I am newbie to the zigbee,I thought buying a
CC2530
ZDK for home automation project. I have following doubts. 1.Does ZStack-ZAP-MSP430-1.0.4.exe contains cc2530-ZNP API libraries? 2.Does CCSv5 is enough to work on ZAP side application ? if yes SO installing ZStack-ZAP-MSP430-1.0.4.exe will includes the libraries for ZNP API's? 3.If I want to modify the ZNP stack,DO i need IAR workbench for 8051?if yes,which Debugger like JTAG i need to use? 4. Does CCSV5 contains IAR plugin ?So that i can work on
cc2530
(ZNP) using CCSv5? 5.Does IAR workbench for 8051 contains CCSv5 plugin?So that I can work on ZAP using IAR Workbench for 8051? 6.Do I need to install IAR for 8051 and CCSv5 to work on ZNP and ZAP respectively ? Thanks, Jagas
Report Abuse
Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.