1351.2.4GHz RF4CE RX_Schematic.pdf5732.2.4GHz RF4CE TX_Schematic.pdf
4314.S-412G RF4CE TX_ CHIP_ANT.zip
When I connect CC debugger to my target board, the status LED has been red.
So I can't program on the SmartRF FLASH programmer.
I think there are some problems on the debugging interface connections.
Would you please examine my schematic and gerber attached?
thank you.
Hi,
your debug connection from a schematic point of view looks correct.
Let’s verify few steps for the sake of clarity:
Thanks,
TheDarkSide
Thanks for your reply!
In case of CC Debug connection test with CC2533 RF4CE Basic Development kit, there are no problem.
the problem is connection with Target board and CC Debug.
i can not find any wrong point in schematic and PCB gerber file.
could please recommend another check point ?
Thanks
Hi Ko Rak Gon,
Have you remembered to power your board? Pin 2 of the debug interface does _not_ supply power from the debugger to the board.
Your schematic and layout looks correct, however I can not view the drill file. Have you remembered to connect the EGP of the chip to ground through vias?
/Fredrik
--PS. If I answered your question, please hit Verify Answer !