When I compile and download by using the example in RemoTI-CC253xDK-1.21 -- project – RemoTI -- HidDongle to the hardware it cannot work .
The hardware LED blink for 3 times and it will show Not Regconize Device Found in Windows, but when I try to download using hex file by using flash programmer the hardware work fine.
So I wondering there should be another coding that works for this dongle side .
Can we get the working code?
Hi Jason,
It can sometimes be tricky to debug an application which enumerates on the same PC. Would you please try to plug the dongle into a different computer from which you are running the debugging session?
Or are you saying that flashing the device with the IAR project does not work. Even when you unplug and then plug the device back in, or by other means reset it?
Torbjorn
Best regards,
Helps us tracking and improving the quality of our support to the community:
if you were satisfied with the answer and of the support, could you please click on 'Verify this post'?
Jason:
What Windows version are you using? Are you using Windows 7?
LPRF Rocks the World
"Customer Centricity, Enthusiasm, Mass collaboration and Great minds are the best path towards great products"
“Victory awaits him who has everything in order – luck people call it. Defeat is certain for him who has neglected to take the necessary precautions in time; this is called bad luck.” Roald Amundsen, The South Pole
We using IAR project to program into the hardware using the example code in (RemoTI-CC253xDK-1.21 -- project – RemoTI – HidDongle) cannot work. But we using the hex code in below directory to program using TI flash programmer can work.