• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » WLAN Applications Forum » Alter Bluetooth Transmission Power in a WL1271
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

Alter Bluetooth Transmission Power in a WL1271

This question is not answered
Mark Janke
Posted by Mark Janke
on Sep 22 2011 14:30 PM
Prodigy80 points

Hi,

Our current product includes a WL1271 chipset (TiWi-R2 module). We would like to reduce the effective Bluetooth range of our product. Our previous product supported a CSR Bluetooth chip that facilitated range control by altering register values within silicon. Specifically - we would alter a pre-amp power register, transmit power register and the power table register values (remove all table rows except the row stipulating the lowest power). Are there registers within the WL1271 that we can alter upon each startup (dynamic storage) or when each system is setup (static storage) to reduce effective Bluetooth range? We run Linux kernel 2.6.37 and are comfortable issuing HCI commands (including vendor specific commands) using "hcitool cmd". Our hope is that we can simply use HCI_VS_WRITE_HARDWARE_REGISTER along with appropriate register and data values to do what we need. Within another post (http://processors.wiki.ti.com/index.php/Bluetooth_FCC_Mode#WL1271_.2B_ARM_Platforms) we can see details on a vendor specific HCI command (Configure Transmitter Parameters) that is helpful for FCC testing, but this command sets many parameters at once including the "Power Level". We don't need to disable scanning and put the controller into a mode appropriate for testing, we only need to change transmission strength.

Perhaps approching this from another angle is easier. If changing a config file used by the Bluetooth controller will work - we are open to this approach.

Any help is appreciated.

Mark J

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Gustavo L
    Posted by Gustavo L
    on Sep 26 2011 07:44 AM
    Genius9990 points

    Mark,

    Changing the initialization script used by the device is definitively the way to go for you. Can you share the file so I can see what you're using?

     

    Regards,
    Gustavo

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Mark Janke
    Posted by Mark Janke
    on Sep 26 2011 09:28 AM
    Prodigy80 points

    HI Gustavo,

    We have not altered the original script that was supplied with the AM18x EVM that we are using as a reference. I could not even tell you which file holds this script. If you advise which file, I can send you what we are using.

    Thanks,

    Mark J

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gustavo L
    Posted by Gustavo L
    on Oct 13 2011 10:06 AM
    Genius9990 points

    Mark,

    Here is the information on changing the power vector:

    Mattais,

    You need to set power vectors for the individual modulation types (GFSK=0, EDR2=1, EDR3=2) and set the max power levels in a separate command. All in all, that's 4 commands which are also executed by the service patch. You can adapt them to your needs.

    To set the following:
    a) Max Output Power is 12dBm(GFSK) and 10dBm (EDRx)
    b) Min Output Power is -35dBm
    c) Dynamic Range is ~30dBm
    d) Step Size is 5dBm
    e) The number of levels is defined by duplicating the same value in consecutive power levels.
    f) Level 0 is used for BLE/ANT in new devices. For old devices, it should be left as is.
    g) If updating the Power Vectors after loading the service patch, the re-calibration sequence must be sent afterwards.

    For the power vectors, the  command "HCI_VS_DRPb_Set_Power_Vector (0xFF82)" is used.

    The format is: { 0x82, 0xfd, 0x14, modulation type, power level 0, power level 1, ..., power level 15, 0xff, 0x00, 0x00};

    The power levels are given as signed 8-bit integers in 1/2 dBm steps, e.g. to use 10 dB, the value 0x14 (20) has to be specified. Only even values (= integer dBm steps) are possible.
     
    h) The "HCI_VS_DRPb_Set_Class2_Single_Power" (0xFF87) command should be used to pick a power level from the power vectors set before. You should pick the level with greatest value smaller than 4dBm.

    The format is: { 0x87, 0xFD, 0x03, GFSK index, EDR2 index, EDR3 index}

     

    Regards,
    Gustavo

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Mark Janke
    Posted by Mark Janke
    on Jul 10 2012 12:11 PM
    Prodigy80 points

    Hi Gustavo,

    Thanks for the info. We read it after you had posted it and then went looking for a simpler solution. Other priorities came up, but we are finally ready to tackle this issue.

    Our challenge is that we have limited experience dealing with the HCI interface through native "C/C++". Our preference would be to use hcitool to execute required commands.  I could not find any helpful online reference explaining how to call "HCI_VS_DRPb_Set_Power_Vector" or "HCI_VS_DRPb_Set_Class2_Single_Power" (other than some TI scripts established for FCC testing). To define our requirements more ...

    - We only support GFSK (long story).

    - If power vectors are already established for min, max and some intermediate power levels, we don't need to change them and would prefer to simply select a vector. This would simplify our task. Is there an hcitool call (specifying HCI command) that we can make to read GFSK power levels? Explicit hcitool syntax would be great.

    - An example hcitool call to select a GSFK index using "HCI_VS_DRPb_Set_Class2_Single_Power" would help.

    Thanks in advance and all apologies for the delay on continuing this thread.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Mark Janke
    Posted by Mark Janke
    on Jul 13 2012 18:27 PM
    Prodigy80 points

    Well, we have spent considerable time utilizing "hcitool cmd" to try and issue HCI_VS_DRPb_Set_Class2_Single_Power with little success. We feel that if we had a clearly defined OCF value and parameters, we would be able to select a power vector as suggested. The other missing element is an HCI command that would allow us to verify that we actually made a controller power change. We have tried OCF values of 0xFF82, 0xFD82, and 0x0082. Only 0x0082 seems to work, but we don't seem to actually change the power level and the "FD" value provide must be used somewhere. OCF values need to be clarified.

    TI (Gustavo or ??) ... how can we get our hands on the TI specific (OGF=0x3F) HCI commands? The HCI_VS_DRPb_Set_Class2_Single_Power  and HCI_VS_DRPb_Set_Power_Vector values are defined in a header that doesn't even seem to be available to the general public!

    Given that we are now comfortable with issuing hcitool commands, I am confident that if we had OCF and parameter values for selecting a power vector and similar info for determining which vector is selected, we would be able to control power as required. If we also had OCF and parameters for setting power vector values and reading currently set power vector values, we would have even more control. How do we get this info?

    Please help.

    Mark J

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use