Dear All,
I got one TI panda board. I try to debug wifi module.
I find it uses ls240-wi-01-a20 module which should uses TiWi_R2 integrated wl1271 wifi transceiver.
I can get datasheet from http://www.lsr.com/products/radio_modules/802.11/tiwi-r2.aspx,
but the datasheet did not describe operation sequence via SDIO or something else in detail. So I still can not understand how to operate the module.
Where can I get this documentation?
Thank you.
Who can give me a answer?
I'm not sure that you can get these registers description. Since the host-wilink protocol is changes between FW versions.
- Elad.
- Elad Raz
CTO
www.integrity-project.com
Hello,
This is addressed in the TiWi Wiki FAQs & other threads on the 2e2.
http://wiki.lsr.com/TiWi.ashx#FAQ_45
Christopher Hofmeister
LS Research
Hi Christopher,
in the link that you provided there are only FAQ1 to 16, FAQ 45 is not there. is there other link?
Regards,
Eyal
Eyal,
I see the reason for the confusion, that is the auto-generated link to the entire FAQ section, it is not intended to be a link to a specific FAQ.
I was hoping FAQ's #2 and #7 would help the customer.
Chris
Hi Chris,
you are right.
Thanks,