What is the diff wrt SW and HW?
1283 includes 5GHz band to support 802.11a as well.
1281 is b/g/n rates (2.4GHz) only.
Same apply for 1271/1273
- Elad.
- Elad Raz
CTO
www.integrity-project.com
Thanks for your help
So, you mean it effects only to WiFi?
If I have only 1283 libraries, Is it compatible with 1281 for all features(GPS etc)?
and could you list up WiFi related drv/lib?
Hi,
as far as WLAN the binaries will be the same, main difference will be with the nvs file that, as for GPS i will verify
Regards,
Eyal
The WL128x solution is targeted at certain customers and is not broadly available.
Due to this, we are unable to provide details you requested in the public forum.
Please contact your local TI Sales representive or module partner for any support requests related to WL128x.
Adnan
OK
Then, could you explain the nvs file? what is it and what for?
NVS file contains 2 main parts, the first one is RF related parameters that is used by the Calibrator application to calibrate the RF signals, and the second is Driver default parameters .
for more information on the Calibration please refer to http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_Calibration_Proccess_NLCP