Hi All,
We have custom platform based on OMAP4460.
The WiFi module used is wl1271 jorjin. We have used TQS_S_2.6.ini file to calibrate it.
We are seeing some poor performance.
Should the TQS_S_2.6.ini be tuned to get good performance?
Regards,
Krt
Krt,
You can find information about WLAN calibration here: http://omappedia.org/wiki/Android_Mac80211#WLAN_Calibration_Instruction
Regards,Gina
Please click the Verify Answer button on this post if it answers your question
_______________________________________________________
Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ
Hi Gina,
Thanks for the reply , I was aware of manual calibration.
My question was specific to the INI file in use for calibration, is it possible to achieve better performance by tweaking the INI file.
I am moving this thread to the WLAN Applications Forum to better answer.
Please find the INI file for Jorjin WL1271 module. thanks,
Saurabh
But during calibration we are getting error.
root@Vega0:~# ./calibrator plt calibrate[ 8688.601013] wl1271: ERROR command complete timeout[ 8691.218200] wl1271: ERROR command complete timeout[ 8693.827575] wl1271: ERROR command complete timeout[ 8693.838287] wl1271: ERROR firmware boot in PLT mode failed despite 3 retriesFail to set PLT power mode on
Usage: ./calibrator [options] plt calibrate [<single|dual>]
Do calibrate for single or dual band chip
Options: --debug enable netlink debuggingroot@Vega0:~#
[ 8750.869567] wl1271: ERROR firmware boot in PLT mode failed despite 3 retries-- Debug: Received Message:-------------------------- BEGIN NETLINK MESSAGE --------------------------- [HEADER] 16 octets .nlmsg_len = 68 .nlmsg_type = 2 <ERROR> .nlmsg_flags = 0 <> .nlmsg_seq = 1364583621 .nlmsg_pid = 4831 [ERRORMSG] 20 octets .error = -110 "Connection timed out" [ORIGINAL MESSAGE] 16 octets .nlmsg_len = 16 .nlmsg_type = 17 <0x11> .nlmsg_flags = 5 <REQUEST,ACK> .nlmsg_seq = 1364583621 .nlmsg_pid = 4831--------------------------- END NETLINK MESSAGE ---------------------------Fail to set PLT power mode on
Matadeen